Skip to main content
ztymyws
Visitor II
September 15, 2016
Question

Current sensing with inverting amplifier

  • September 15, 2016
  • 1 reply
  • 875 views
Posted on September 15, 2016 at 23:22

Hi,

I have been trying to use FOC SDK 4.2 with existing hardware. The board uses inverting amplifier instead of non-inverting ones. Anyone got an idea on how to modify the code?

So far I've tried:

1. use negative value for amplifier gain:  doesn't work

2. use negative value for current shunt:   doesn't work

3. use negative gains for the current loops:  stable current loop, but will trigger ''speed feedback'' fault.

Thanks!

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards