cancel
Showing results for 
Search instead for 
Did you mean: 

Best method to measure temperature of STSPIN32G4

FedericoHW
Associate

Hi,

I made some temperature measures on STSPIN32G4 using a thermal camera.

I saw that the central part 3x3mm of the STSPIN reaches about 70°C, while the sorrounding part does not go beyond 50°C.

My question is the following: if I use the internal temperature sensor I will read the temperature of the central part or the sorrounding part?

 

Thank you

Federico

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Cristiana SCARAMEL
ST Employee

Hello @FedericoHW and welcome to the ST Community.

I confirm that the internal temperature sensor reports the temperature of the device central part.

If you feel a post has answered your question, please click "Accept as Solution"

View solution in original post

1 REPLY 1
Cristiana SCARAMEL
ST Employee

Hello @FedericoHW and welcome to the ST Community.

I confirm that the internal temperature sensor reports the temperature of the device central part.

If you feel a post has answered your question, please click "Accept as Solution"