Skip to main content
Associate
Jan 11, 2024 7:39 PM UTC
Question

AC induction Motor for New Project

Hello;

I want to create  Ac induction motor project. So I cannot find ACIM GUI or ACIM profile in MC Workbench any versions. Could you please give an answer for my questions

1. Can i download ACIM GUI ?

2. Can i find a acim profile  for mc workbench 

3. How do i put Acim Selni Ahv 242 to my project 

Regards 

Motor Workbench  6.2.1

Stm32cubemx 6.10.0

Control board: NUCLEO-G431RB

Power Board: STEVAL-IPM30B

9 replies

cedric H
ST Technical Moderator
Jan 15, 2024 1:47 PM UTC

Hello @ariftukel ,

Our ACIM offers is currently limited to the following configuration: NUCLEO-G431RB and STEVAL-IHM023V3.

It can be run only through the example list as highlighted below.

cedricH_0-1705326169109.png

We plan to add the full support of the ACIM algorithm for September 2024.

Regards

Cedric

Visitor II
Nov 8, 2024 6:49 PM UTC

 Hi, what is the status for adding the full support of the ACIM algorithm plan? When will it be added? sorry for bad eng :) thx.

Gael A
ST Employee
Nov 11, 2024 8:36 AM UTC

Hello Demir42,

I am sorry to inform you that full ACIM support has been postponed. Though it is still on our roadmap, I cannot give you any precise information on when it will be released.

We apologise for the inconvenience.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.
ariftukelAuthor
Associate
Jan 21, 2024 5:36 PM UTC

Thank you for everything . I will try with them.

blechleitner
Associate II
Oct 2, 2025 8:44 AM UTC

Hi,

almost one year later, we have now MCSDK 6.4.1, but still no full support for ACIM. Are there any news on this issue?

Maybe someone from ST can explain to the community what are the real reasons for the delayed support for the so far well established ACIM technology and give some insights what we can expect.

Interestingly, in MCSDK 6.3.2, there are at least two examples with ACIM. But the examples disappeared again in MCSDK 6.4.x. 

For me, it looks like we have to go to other silicon vendors to find proper solutions for our project. This would not be the way, we'd like to go, but...

Thanks and have a great day,
Bernhard L.

GMA
ST Technical Moderator
Oct 13, 2025 12:33 PM UTC

Hello @blechleitner,

The ACIM example will be available in MCDSK6.4.2, which is planned for release at the end of 2025.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
blechleitner
Associate II
Dec 18, 2025 8:28 AM UTC

Hi,

in the meantime, we have almost the end of "End of 2025" and we see still no indication, when the full support for ACIM motors will be available. When will MCSDK 6.4.2 be available and will it have the full ACIM support including Motor Profiler?

The only aternative, that keeps being mentioned is the 3-4 years old version 5.Y, but this is no longer offered for download. Is ther a possibility to get a download link?

Are there other possibilities in the STM32 eco system?

Thanks and best regard,

Bernhard L.

 

GMA
ST Technical Moderator
Dec 18, 2025 1:05 PM UTC

Hello @blechleitner,

Thank you for your feedback and your long-term interest in our products. Due to internal constraints, the MCSDK 6.4.2 release that includes the ACIM example is postponed to early 2026.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
Visitor II
Dec 19, 2025 4:08 PM UTC

At this time Motor Workbench does not include a generic ACIM GUI or a dedicated “ACIM profile” in the 6.x series, ST’s AC induction motor support is only available through specific example projects (e.g., ACIM-NUCLEO-G431RB-IHM023V3 in the older X-CUBE-MCSDK 5.x, where an ACIM GUI tool lives under Utilities/PC_Software/ACIMGUI for tuning), and full ACIM support wasn’t carried forward into the 6.2.1 Workbench itself, so you won’t find a simple profile to drop into your project and have to start from those examples and adjust for your SELNI AHV 242 motor.


Related ST forum thread that can help more: https://community.st.com/t5/stm32-mcus-motor-control/acim-and-nucleo-g431rb/td-p/623362/eaguaranteedrent