Question
I am having an issue in the code generated from X-CUBE-AI library. STM32WB55RGxx, using (.onnx)file
Thank you!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
The error are:
TEMPLATE - initialization
TEMPLATE - Error (ai_network_create_and_init) - type=0x33 code=0x41



and I also have another issue is when I using .h5 file to generate .c from X-CUBE-AI library, STM32CUBEMX
Analyzing model warning
E010(InvalidModelError): Model file is not a HDF5 file: E:\AST32WB55PACK\1\3.2-xgb_classifier_model.h5