cancel
Showing results for 
Search instead for 
Did you mean: 

Enabling STM32H745ZI-Q AXI SRAM to store Network Activations

OSala.1
Associate II

I am using the STM32H745ZI-Q Dual Core MCU.

My workflow is to generate the AI library using a Single Core processor and then copy the project into my Dual Core.

Now I am trying to use External Ram Configuration (STMCube) to map the activations NOT into a external RAM but into another Bank (AXI SRAM for example. Address: 0x30000000) but without any luck.

Is there any way I can allocate the Activation buffer on another RAM Bank?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0