2022-08-21 12:56 AM
Noob question - can I use AI with the STM32WL SoC ?
I want to train a model and then use STM32Cube.AI to put it on STM32WLE5CC. This is so I can use AI on the end device and transmit data using LoRa all using the one chip.
Is this possible ?
Many thanks in advance.
Solved! Go to Solution.
2022-08-22 2:16 AM
Yes STM32Cube.AI is supported on the STM32WL MCUs
Regards
Daniel
2022-08-22 2:16 AM
Yes STM32Cube.AI is supported on the STM32WL MCUs
Regards
Daniel
2022-08-23 7:14 PM
Awesome thank you!