AI relocatable run-time API lets the MCU HardFault.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-09-27 10:12 PM - last edited on 2024-07-24 3:22 AM by Amel NASRI
Hi,
I'm testing running a relocatable binary model.
But when I use ai_rel_network_run(), I get into HardFault.
The detailed error information is as follows, with my current test code attached.
Does anyone know how to fix this please?
Thanks in advance.
/* USER CODE BEGIN PV */
float aiInData[AI_NETWORK_IN_1_SIZE];
float aiOutData[AI_NETWORK_OUT_1_SIZE];
const char* activities[AI_NETWORK_OUT_1_SIZE] = {
"stationary", "walking", "running"
};
ai_i32 batch;
ai_handle net = AI_HANDLE_NULL;
ai_handle weights_addr;
ai_bool res;
ai_network_report net_info;
AI_ALIGNED(4) ai_u8 rt_ai_ram[2596*4];
AI_ALIGNED(4) ai_u8 act[1708*4];
/* USER CODE END PV */
Main:
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_CRC_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
ai_error err;
ai_rel_network_info rt_info;
const ai_handle bin_addr = ai_network_reloc_img_get();
err = ai_rel_network_rt_get_info(bin_addr, &rt_info);
//rt_ai_ram = (uint8_t*)malloc(rt_info.rt_ram_xip);
err = ai_rel_network_load_and_create(bin_addr, rt_ai_ram, rt_info.rt_ram_xip,
AI_RELOC_RT_LOAD_MODE_XIP, &net);
//act = (uint8_t*)malloc(rt_info.acts_sz);
if (rt_info.weights)
weights_addr = rt_info.weights;
else
weights_addr = "";
const ai_handle act_addr = act;
res = ai_rel_network_init(net, weights_addr, act_addr);
res = ai_rel_network_get_report(net, &net_info);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
uint32_t write_index = 0;
while (1)
{
aiInData[write_index + 0] = 0.03025;
aiInData[write_index + 1] = 0.1865;
aiInData[write_index + 2] = 0.205;
write_index += 3;
if (write_index == AI_NETWORK_IN_1_SIZE) {
write_index = 0;
printf("Running inference\r\n");
AI_Run(aiInData, aiOutData);
/* Output results */
for (uint32_t i = 0; i < AI_NETWORK_OUT_1_SIZE; i++) {
printf("%8.6f ", aiOutData[i]);
}
uint32_t class = argmax(aiOutData, AI_NETWORK_OUT_1_SIZE);
printf(": %d - %s\r\n", (int) class, activities[class]);
HAL_Delay(500);
}
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
AI_Run():
static void AI_Run(float *pIn, float *pOut)
{
ai_i32 batch;
ai_error err;
ai_buffer *ai_input = net_info.inputs;
ai_buffer *ai_output = net_info.outputs;
ai_input[0].data = AI_HANDLE_PTR(pIn);
ai_output[0].data = AI_HANDLE_PTR(pOut);
batch = ai_rel_network_run(net, ai_input, ai_output);
if (batch != 1) {
err = ai_rel_network_get_error(net);
}
}
And I had already increased both heap and stack size, but the problem still exists.
- Labels:
-
STM32CubeAI
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-09-28 1:38 PM
Hello WHUAN,
What is the version of X-CUBE-AI tools used?
Since 7.1, the multi-heap feature has introduced an API break to initialize the model.
ai_rel_network_init() expects now a table of pointer for the weights and also for the activations.
ai_handle net = AI_HANDLE_NULL;
ai_handle weights_addr;
ai_handle activations;
...
const ai_handle acts[] = { activations };
res = ai_rel_network_init(net, &weights_addr, acts))
...
}
br,
Jean-Michel