Skip to main content
Associate II
January 25, 2024
Question

X-CUBE-AZRTOS packs are missing full folders to make some examples work

Hello community,

I have went around the latest X-CUBE-AZRTOS packs of several MCU series to do some benchmarking and started to install a few software examples to use them in STM32CubeIDE 1.14.0.

I found out that for some of them, the tool fails to copy through the Target Example Selector and therefore they are impossible to build. I digged a little what could be wrong and discovered that all these examples need some files that are not present in the X-CUBE-AZRTOS pack itself, whereas they are present in the related STM32Cube_FW pack !

  • Middlewares/ST/STM32_Audio
  • Utilities/Fonts

This problem exists for the following packs / examples:

  • X-CUBE-AZRTOS-F4 version 1.1.0
    • STM32469I-Discovery/Applications/FileX|ThreadX|USBX/*  (13 examples)
  • X-CUBE-AZRTOS-G0 version 1.1.0
    • STM32G0C1E-EV/Applications/USBPD|USBX/* (7 examples)
  • X-CUBE-AZRTOS-WB version 2.0.0
    • STM32WB5MM-DK/Applications/FileX|ThreadX|USBX/* (3 examples)

The easy workaround for me is to copy these 2 folders from STM32Cube_FW to X-CUBE-AZRTOS, but it obviously needs correction from ST to add what is missing.

Can you confirm it will be done in next pack deliveries ?

This topic has been closed for replies.

5 replies

ST Technical Moderator
January 26, 2024

Hello @Oskar_H 

It is mentioned in Azure RTOS packages:

The scope of this package covers the following Azure RTOS middleware: RTOS (ThreadX), USB Device and Host (USBX), File System including NOR/NAND memories support (FileX and LevelX) and Networking including Ethernet and WiFi media (NetXDuo).

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Oskar_HAuthor
Associate II
January 26, 2024

Hello @FBL 

yes of course, I already know that, and precisely because I wanted to build some examples using FileX, ThreadX, NetXDuo and USBX included in these packs, I faced the copy/build issues I mentionned in this other post : https://community.st.com/t5/stm32cubeide-mcus/fail-to-perform-local-copy/m-p/622589#M22991

None of these examples work when installing with Example Selector of STM32CubeIDE 1.14.0 !

These 3 X-CUBE packs are incomplete, please fix them.

ST Technical Moderator
January 26, 2024

Hello @Oskar_H 

I have tried to reproduce on my side but the build is successful for the example :

  • X-CUBE-AZRTOS-WB version 2.0.0
    • STM32WB5MM-DK/Applications/FileX|ThreadX|USBX/* (3 examples)

FBelaid_0-1706276691680.png

If possible, to share steps to reproduce the issue. On my side I downloaded x cube package from MX tool without issues.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL