Question
Virtual COM port (USB CDC) example - ... Endpoints? _SOLVED but SEVERE MISTAKE in RL-USB!
Posted on July 09, 2011 at 23:13
Hello!
I've adjusted the Virtual Com Port example from the FS USB Library V3.2.1/V3.3.0 to my needs on STM32F103RC. It works. As a preparation to merge USB CDC and Mass Storage (suggestions and solutions are welcome!) I'm trying now first to ''move'' the COM communication to the endpoints 4,5 and 6 instead of the origin 1,2 and 3 in the example. It does not work. Exactly, the Virtual COM does appear under Win7 (endpoint 0 is untouched) but no communication occures. I think I've missed some substitution or misunderstood the allocation of the endpoints. Could anyone share with me a kind of check list, what changes/substitutions should be made to the application part of the USB library (usb_conf.h, usb_desc (.h, .c),usb_prop (.h, .c), usb_endp.c, usb_istr (.h,.c) and
usb_pwr (.h, .c)) to get the communication over EP4, EP5 and EP6? TIA. #usb-endpoints-change #virtual-com-port-alternative-endpoints #composite-virtual-com #usb-cdc-rl-usb-severe-mistake