Skip to main content
RMcCo.2
Associate
December 7, 2021
Question

USB problem

  • December 7, 2021
  • 3 replies
  • 806 views

Gooday

I have a steering wheel which has buttons programmed with an stm32 blue pill board.... my problem is

The board is only recognised on my pcs front USB ports ......any USB ports on the back side of the board give an error (cannot recognise and ports reset failed )​...please is there a specific driver I need or how can I fix this

This topic has been closed for replies.

3 replies

TDK
December 7, 2021

Wouldn't that indicate a problem with your USB ports rather than a problem with the STM32 board?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Pavel A.
December 7, 2021

While waiting for more useful answers:

Get a powered USB 2.0 hub (high speed or full speed, not USB 3.x) and connect your device thru it.

Unless your PC runs Windows 7. Then upgrade :)

RMcCo.2
RMcCo.2Author
Associate
January 26, 2022

I have the exact same problem seems its something to do with the STM32 board