Skip to main content
NRoma.6
Associate
Jul 11, 2022 10:50 AM UTC
Question

USB connection between STM32F411 and modem RM500 quectel

Hi I am working on a project where a need to send AT commands through my MCU to a modem, the problem is that this modem only has a USB interface and not a UART interface, so I have a lot of doubts of how should I do this, i wanted to use the USB_Host_Library but I dont know hot to send the data to a certain interface and enpoint, since que AT command interface appears as a virtual COM (Interface 2 with 3 endpoints).

0693W00000QKqrQQAT.pngAnd which class should I use? Communication Host class?

Thanks in advice, Nicolas.

This topic has been closed for replies.

3 replies

Sundar6444
Graduate
Aug 5, 2024 9:43 AM UTC

Hello Nicolas,

 

Were you able to figure out this? I am also trying to interface the STM32 with Quectel RM500Q and would like to know more about this topic. 

 

Thanks in advance

Sundar.

Andrew Neil
Super User
Aug 5, 2024 10:14 AM UTC

Similar recent question here:

https://community.st.com/t5/stm32-mcus-embedded-software/can-t-enumerate-telit-modem-usb-port-as-a-cdc-acm-device-with/m-p/704856#M50143

 


@Sundar6444 wrote:

trying to interface the STM32 with Quectel RM500Q .


Have you contacted Quectel for support with that?

Maybe they can suggest tips for interfacing this module to microcontrollers?

Maybe they can suggest a solution better suited for microcontroller connection?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Sundar6444
Graduate
Aug 5, 2024 2:04 PM UTC

@Andrew Neil 

Thanks for sharing the link. It seems a lot of members are trying to interface STM controllers with modems.

Yes, i approached Quectel and looks like it is a dead end. They have asked me to develop a driver ourselves.