Skip to main content
Robin7331
Associate
Apr 7, 2021 9:39 AM UTC
Solved

Unable to run STM32F401 at 84 MHz Sysclk (works fine at 48 MHz)

Hello guys :waving_hand:

​

I am having a STM32F401CDU6TR on a custom board and I am not able to run it at 84 MHz SYSCLK. The source is an external 8 MHz crystal with two 22pF caps as seen here:

0693W000008yrF6QAI.png​

I created the project in CubeMX as a Makefile project. I only use CubeMX for configuring the GPIOs as well as the clock. The actual code is written and flashed via VSCode. Works great so far.

​

Here is my current 84 MHz clock configuration in CubeMX:

0693W000008yrFzQAI.pngAnd this is my RCC configuration:

0693W000008yrHCQAY.png​

When I flash this code I always end up in a HardFault_Handler before the SystemClock_Config(); function returns.

​

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 8;
 RCC_OscInitStruct.PLL.PLLN = 336;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
 RCC_OscInitStruct.PLL.PLLQ = 7;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 Error_Handler();
 }
}

When I activate MCO1 I can measure the HSE and PLLCLK signals with the expected frequency.

When I set the SYSCLK to 48 MHz as seen here everything works as expected.

0693W000008yrOSQAY.png 

I have no idea what is going on here 🤷�?♂�?

Thanks for your help!

Cheers,

Robin

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Apr 7, 2021 12:29 PM UTC

Should be at least 2.2 uF, it is a bulk capacitor for the internal LDO

I'll double check the specs, the single up case might be 4.7 uF

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

21 replies

waclawek.jan
Super User
Apr 7, 2021 10:40 AM UTC

> When I flash this code I always end up in a HardFault_Handler before the SystemClock_Config(); function returns.

Single-step that code, best in disasm view (i.e. instruction by instruction) to find out where it goes into the HardFault.

Is FLASH set appropriately to your VDD and clock? Is VDD stable enough? Do you have adequate decoupling?

Try the same code on a "known good" board such as Nucleo or Disco.

Is your crystal 8MHz?

JW

Andrew Neil
Super User
Apr 7, 2021 10:43 AM UTC

"8 MHz crystal with two 22pF caps"

It actually shows 20pF

and the crystal is labelled "16pF"

Is it actually oscillating at all? If it is, is it at 8MHz?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Robin7331
Robin7331Author
Associate
Apr 7, 2021 11:29 AM UTC

Thanks for taking time! Here are my answers.

> Single-step that code, best in disasm view (i.e. instruction by instruction) to find out where it goes into the HardFault.

Will do that later this day. Thanks.

> Is FLASH set appropriately to your VDD and clock?

I am not sure what you mean by that? The voltage of the flash? How do I set that?

​

> Is VDD stable enough?

I am not sure what is considered stable. I'll do some measurements later while powering on the board.

I am looking for a voltage drop on that line? And or jitter?

​

> Do you have adequate decoupling?

I placed 100n decoupling caps across all VDD/GND supply pins around the MCU as close to the MCU as possible.

I might be able to refactor this so the caps are closer. But when I take a look at a nucleo board those seem to be even further away from the MCU.

But I have to admit that my decoupling design could be better. Do you think that is the issue?

Here's a picture of the board layout with the 3v3 net highlighted. Back copper is hidden. Its a 4 layer board.

0693W000008ysIfQAI.png​

> It actually shows 20pF

You're right. I meant to say 20 pF. Thats what I have installed.

​

> Is it actually oscillating at all? If it is, is it at 8MHz?

It is oscillating at exactly 8 MHz. The only thing that bothers me is the voltage peak to peak is a little low, right?

Might also be because I am introducing an error when measuring with my 10x probe.

I measured at one of the crystals leads.

0693W000008ys6FQAQ.jpg​

Tesla DeLorean
Guru
Apr 7, 2021 11:42 AM UTC

HSE looks fine

W​hat's going on with VCAP? Check voltage and capacitor value.

Should see 1.25V​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Robin7331
Robin7331Author
Associate
Apr 7, 2021 12:04 PM UTC

> W​hat's going on with VCAP? Check voltage and capacitor value.

The value is 2.2n as seen here

0693W000008ysXzQAI.png​

Thats what I see when measuring on the MCU facing side of the C9. Seems fine, right?

0693W000008ysY9QAI.jpg​

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Apr 7, 2021 12:29 PM UTC

Should be at least 2.2 uF, it is a bulk capacitor for the internal LDO

I'll double check the specs, the single up case might be 4.7 uF

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
Apr 7, 2021 12:36 PM UTC

0693W000008ysjqQAA.jpg

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Robin7331
Robin7331Author
Associate
Apr 7, 2021 12:39 PM UTC

Oh you are right!

Thats clearly a bug.

Thanks for pointing it out. Will swap that for a 4.7uF one.

waclawek.jan
Super User
Apr 7, 2021 12:40 PM UTC

I hate how Clive always beats us all in this game... must be the inferior quality of my crystal cube... ;)

Jan

Tesla DeLorean
Guru
Apr 7, 2021 12:50 PM UTC

Mine's more of a tesseract than a cube..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
DavidAlfa
Senior II
Apr 7, 2021 1:51 PM UTC

Did you check that at least something is working?

Debug it and ensure that the mcu is actually running.

Tesla DeLorean
Guru
Apr 7, 2021 3:37 PM UTC

Please at least pay attention, the top post indicates it runs at a lower speed.

And the problem was solved/addressed before you posted.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Robin7331
Robin7331Author
Associate
Apr 7, 2021 2:24 PM UTC

Guys. It works! :party_popper:

The problem was that I took the wrong cap value for VCAP.

I took 2.2nF instead of 4.7uF.

Now, there is no problem anymore with having a SYSCLK of 84 MHz.

Thanks for the heads up @Community member​ 

You made my day :waving_hand:

0693W000008ytjJQAQ.png

DavidAlfa
Senior II
Apr 7, 2021 2:47 PM UTC

It's magic that it worked with only 2.2nF :D

Robin7331
Robin7331Author
Associate
Apr 7, 2021 3:09 PM UTC

Absolutely. But it had another problem as well. USB DFU was not working.

And sometimes BOOT0 = HIGH was not recognized and it would boot right into flash instead of using the integrated bootloader.

All those problems: vanished 🤩✌�?

And it makes sense when I think about it now. I am super glad that his fixed all those issues ;p

DavidAlfa
Senior II
Apr 7, 2021 3:15 PM UTC

I've seen that problem in the 32F411 "black pills".

Apparently the crystal starting is too slow when cold.

And how to fix it? Put the finger on top of the mcu for a few seconds to warm it up, then connect, it works everytime!

It might be caused by a cheap chinese magic too.