Skip to main content
BengofEtech
Associate III
April 2, 2020
Question

STMH7 ETH_DMAMR_SWR fails

  • April 2, 2020
  • 4 replies
  • 3668 views

Hey,

i got a specific Problem with the STM32H7 Ethernet, sometimes when performing

 SET_BIT(heth->Instance->DMAMR, ETH_DMAMR_SWR);
 
 /* Get tick */
 tickstart = HAL_GetTick();
 
 /* Wait for software reset */
 uint8_t force_reset = 0;
 while (READ_BIT(heth->Instance->DMAMR, ETH_DMAMR_SWR) > 0U)
 {
 if(((HAL_GetTick() - tickstart ) > ETH_SWRESET_TIMEOUT))
 {
 /* Set Error Code */
 heth->ErrorCode = HAL_ETH_ERROR_TIMEOUT;
 /* Set State as Error */
 heth->gState = HAL_ETH_STATE_ERROR;
 /* Return Error */
 return HAL_ERROR;
 break;
 }
 }

The error gets detectet, so ETH_DMAMR_SWR doesnt get activated within this timeout period. Is there aother way to reset the ETH Controller except from restarting the whole mcu?

I tried __HAL_RCC_ETH1MAC_FORCE_RESET but it didnt work out.

This topic has been closed for replies.

4 replies

BengofEtech
Associate III
April 2, 2020

okay much more interesting:

 /* Get tick */
 tickstart = HAL_GetTick();
 
 /* Wait for software reset */
 uint8_t force_reset = 0;
 while (READ_BIT(heth->Instance->DMAMR, ETH_DMAMR_SWR) > 0U)
 {
 if(((HAL_GetTick() - tickstart ) > ETH_SWRESET_TIMEOUT))
 {
 /* Set Error Code */
 heth->ErrorCode = HAL_ETH_ERROR_TIMEOUT;
 /* Set State as Error */
 heth->gState = HAL_ETH_STATE_ERROR;
 /* Return Error */
 force_reset = 1;
 break;
 }
 }
 
 
 tickstart = HAL_GetTick();
 if(force_reset)
 {
//	 tickstart = HAL_GetTick();
	 __HAL_RCC_ETH1MAC_FORCE_RESET();
	 HAL_Delay(100);
	 __HAL_RCC_ETH1MAC_RELEASE_RESET();
	 HAL_Delay(100);
	 SET_BIT(heth->Instance->DMAMR, ETH_DMAMR_SWR);
	 while (READ_BIT(heth->Instance->DMAMR, ETH_DMAMR_SWR) > 0U)
	 {
	 if(((HAL_GetTick() - tickstart ) > ETH_SWRESET_TIMEOUT))
	 {
	 /* Set Error Code */
	 heth->ErrorCode = HAL_ETH_ERROR_TIMEOUT;
	 /* Set State as Error */
	 heth->gState = HAL_ETH_STATE_ERROR;
	 /* Return Error */
 
	 return HAL_ERROR;
	 }
	 }
 }

when optimising AND uncomment the tickstart, the whole programm wont run correctly. Anyone expirienced things like that?

BengofEtech
Associate III
April 2, 2020

there seems something wrong with data alligmnent. cant imagine, it could be something written on the flash. any experiences?

as far as i can tell, usually adding non related code in flash should not interfere with the programs ability to function, which is clearly the case here.

Associate
October 27, 2023

I have run into the same issue with my STM32H753 MCU(https://community.st.com/t5/stm32-mcus-products/stm32h753-ethernet-initialization-failure/td-p/602033)

Were you able to fix this issue?

Graduate
October 30, 2024

Same issue here on a H747 DISC0. Same c-code as yesterday, starting my program today and constantly running into this behaviour.

This line of code triggers the Hardfault_Handler()

SET_BIT(heth->Instance->DMAMR, ETH_DMAMR_SWR);

But when debugging I noticed that this function is called already by MX_ETH_Init (I guess so). So the SET_BIT function was called already and is running into the HardFault_Handler, when called the second time.
After commenting out "HAL_ETH_Init(&heth)" in my main.c, I didn't run into the error any more :)

 

Still wondering why I didn't run into the HardFault_Handler yesterday, when HAL_ETH_Init" was called twice (1x MX Init + 1x main.c)

Hope this will help anyone :)
Cheers