Skip to main content
Penguins
Associate
June 19, 2025
Solved

STM32G4xx HAL Driver V1.2.5 Issue with DMAMUX

Hello ST,

I would like to report a bug in the <stm32g4xx_hal_dma.c> file (V1.2.5). In the function DMA_CalcDMAMUXChannelBaseAndMask(DMA_HandleTypeDef *hdma), there's an error in calculating hdma->DMAmuxChannelStatusMask. For DMA2 channels, the channel_number should be adjusted by adding 8, 6, or 7 according to the MCU category. Otherwise, it will NOT be able to correctly determine and clear the synchronization overrun interrupt of the corresponding channel.

To give you a better understanding of the issue, I've included some relevant code snippets with comments at Line 32 below:

/**
 * @brief Updates the DMA handle with the DMAMUX channel and status mask depending on stream number
 * @PAram hdma pointer to a DMA_HandleTypeDef structure that contains
 * the configuration information for the specified DMA Stream.
 * @retval None
 */
static void DMA_CalcDMAMUXChannelBaseAndMask(DMA_HandleTypeDef *hdma)
{
 uint32_t dmamux_base_addr;
 uint32_t channel_number;
 DMAMUX_Channel_TypeDef *DMAMUX1_ChannelBase;

 /* check if instance is not outside the DMA channel range */
 if ((uint32_t)hdma->Instance < (uint32_t)DMA2_Channel1)
 {
 /* DMA1 */
 DMAMUX1_ChannelBase = DMAMUX1_Channel0;
 }
 else
 {
 /* DMA2 */
#if defined (STM32G471xx) || defined (STM32G473xx) || defined (STM32G474xx) || defined (STM32G414xx) || defined (STM32G483xx) || defined (STM32G484xx) || defined (STM32G491xx) || defined (STM32G4A1xx) || defined (STM32G411xC)
 DMAMUX1_ChannelBase = DMAMUX1_Channel8;
#elif defined (STM32G411xB) || defined (STM32G431xx) || defined (STM32G441xx) || defined (STM32GBK1CB)
 DMAMUX1_ChannelBase = DMAMUX1_Channel6;
#else
 DMAMUX1_ChannelBase = DMAMUX1_Channel7;
#endif /* STM32G4x1xx) */
 }
 dmamux_base_addr = (uint32_t)DMAMUX1_ChannelBase;
 channel_number = (((uint32_t)hdma->Instance & 0xFFU) - 8U) / 20U;
 /** Code should be added here to distinguish DMA2 channels from DMA1 ones. **/
 hdma->DMAmuxChannel = (DMAMUX_Channel_TypeDef *)(uint32_t)(dmamux_base_addr + ((hdma->ChannelIndex >> 2U) * ((uint32_t)DMAMUX1_Channel1 - (uint32_t)DMAMUX1_Channel0)));
 hdma->DMAmuxChannelStatus = DMAMUX1_ChannelStatus;
 hdma->DMAmuxChannelStatusMask = 1UL << (channel_number & 0x1FU);
}

Best regards,
Penguins

Saket_OmBest answer
ST Technical Moderator
June 20, 2025

Hello @Penguins 

Thank you for bringing this to our attention 

I reported this internally 

Internal ticket number: 212655 (This is an internal tracking number and is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om

4 replies

Saket_OmBest answer
ST Technical Moderator
June 20, 2025

Hello @Penguins 

Thank you for bringing this to our attention 

I reported this internally 

Internal ticket number: 212655 (This is an internal tracking number and is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Penguins
PenguinsAuthor
Associate
November 22, 2025

I noticed that this issue has not been fixed yet.

ST Technical Moderator
November 24, 2025

Hello @Penguins 

The fix is scheduled to be released on GitHub soon.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om