Skip to main content
doubleset
Associate
Mar 4, 2022 8:27 AM UTC
Solved

STM32G431 TS_CAL2 temperature

HI

At what temperature the TS_CAL2 value for the STM32G431 is detected?

In the datasheet it is reported 130 degrees while in the library "stm32g4xx_ll_adc.h" TEMPSENSOR_CAL2_TEMP is 110 degrees

Thanks

This topic has been closed for replies.
Mike_ST
Mike_STBest answer
ST Technical Moderator
Mar 4, 2022 10:16 AM UTC

Hello,

Correct answer is 130°C

You're probably using STM32G4 firmware package below version 1.5.0, where it is updated.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 

7 replies

Mike_ST
Mike_STBest answer
ST Technical Moderator
Mar 4, 2022 10:16 AM UTC

Hello,

Correct answer is 130°C

You're probably using STM32G4 firmware package below version 1.5.0, where it is updated.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
jacobq
Associate II
Sep 24, 2024 5:56 PM UTC

Has this been fixed? It appears to still be incorrectly specified as 110C in STM32Cube FW_G4 V1.6.0

See https://github.com/STMicroelectronics/stm32g4xx_hal_driver/issues/20

Explorer
Sep 9, 2025 12:55 PM UTC

I don't think it has been fixed.. Had to hardcode it to 130UL myself..

doubleset
doublesetAuthor
Associate
Mar 4, 2022 11:31 AM UTC

Right, thanks,

For the G431 I'm using STM32CubeIDE Version 1.7.0 with STM32Cube FW_G4 V1.4.0 because using STM32CubeIDE Version 1.8.0 with STM32Cube FW_G4 V1.5.0 and the same code the interrupts are not generated or intercepted and I don't understand why

Amel NASRI
ST Technical Moderator
Mar 11, 2022 10:24 AM UTC

Hi @doubleset​ ,

New versions for STM32CubeIDE & STM32CUbeMX are currently available. If the issue with interrupts you introduced previously is still there, please describe it with more details in a new post. It will be helpful in order to anlayze & fix it.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Associate III
Sep 18, 2025 9:14 AM UTC

It is 130 deg.