TbubVisitor IIForum|Forum|7 years agoSeptember 9, 2019QuestionSTM32CubeMX L4 V1.13.0 HAL_OSPIM_Config corrupts port configuration.Forum|Forum|7 years agoSeptember 9, 20190 replies676 viewsWe are using STM32Cube_FW_L4_V1.13.0 and ran into trouble using two Octo SPI controllers with one running in Octo and one running in Quad mode.While configuring the Quad mode IO ports with HAL_OSPIM_Config the configuration of the second one got corrupted. Had to patch the stm32l4xx_hstm32l4xx_hal_ospi-c.zipBug-reportOctoSPISTM32L4 seriesSTM32Cube MCUs packages