Skip to main content
Associate II
February 24, 2026
Solved

sharing data between two cores of H7 with FreeRTOS

Title edited - originally said, "sharing data between two boards"


Good day y'all,

I'm trying for the first time to have the two cores on a H7 board share data between one another on shared memory, in particular cm7 writing data and cm4 read it. 
From what I understand I need to use a semaphore to signal back and forth to alert the cm4 when there is new data in every iteration, the theory I get, but I'm not sure of the shared memory allocation and the semaphore correct availability. Is there any example code I can see to understand how it's supposed to go? I tried looking at the ide examples, but anytime I try to open the example folder the ide application just dies :\ 

Thx all for the advices, 

P.S. I'm also using FREERTOS but it's not supposed to cause any problem but you never know 

6 replies

Andrew Neil
Super User
February 24, 2026

@Jack_DB Your title says, "sharing data between two boards", but you actually seem to be talking about sharing data between the cores in one chip - therefore on the same board ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Jack_DBAuthor
Associate II
February 24, 2026

Yeah sorry misspoke, I meant two cores... 

Andrew Neil
Super User
February 24, 2026
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Technical Moderator
February 25, 2026

Almost the same question asked in this post: How can I bridge between two cores in STM32H745 to share data?

As you are using FreeRTOS, from the AN5617: the usage of stream buffer/message buffer in FreeRTOS context:

screenshot.png

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
February 25, 2026

@Jack_DB wrote:

P.S. I'm also using FREERTOS  


So take a look what facilities FreeRTOS itself provides for inter-processor comms & multiple cores; eg,

Multicore advice and suggestions

Simple Multicore Core to Core Communication Using FreeRTOS Message Buffers

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.