Skip to main content
Associate II
Feb 28, 2024 11:52 AM UTC
Question

Sending encoder data to terminal as CDC device without UART

 

 

Hi everybody, 

My project is reading encoder data, and then send this data to the terminal via USB connection. As transmit and receive I want to use CDC_Transmit and CDC_Receive function. But no matter what I do, I cannot see the encoder data in the terminal. My code and configurations are below: 

 

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "usb_device.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
TIM_HandleTypeDef htim3;

/* USER CODE BEGIN PV */
uint32_t encoder_value;
char encoder_buffer[200];
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_TIM3_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_TIM3_Init();
 MX_USB_DEVICE_Init();
 /* USER CODE BEGIN 2 */
	HAL_TIM_Base_Start_IT(&htim3);
	HAL_TIM_Encoder_Start_IT(&htim3, TIM_CHANNEL_ALL);
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
	 encoder_value = TIM3->CNT;
	 sprintf(encoder_buffer, "first encoder: %d\n\r", encoder_value);
	 CDC_Transmit_FS((uint8_t*)encoder_buffer, sizeof(encoder_buffer));
	 HAL_Delay(500);

 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL6;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USB;
 PeriphClkInit.UsbClockSelection = RCC_USBCLKSOURCE_PLL;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief TIM3 Initialization Function
 * None
 * @retval None
 */
static void MX_TIM3_Init(void)
{

 /* USER CODE BEGIN TIM3_Init 0 */

 /* USER CODE END TIM3_Init 0 */

 TIM_Encoder_InitTypeDef sConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};

 /* USER CODE BEGIN TIM3_Init 1 */

 /* USER CODE END TIM3_Init 1 */
 htim3.Instance = TIM3;
 htim3.Init.Prescaler = 0;
 htim3.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim3.Init.Period = 65535;
 htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
 sConfig.EncoderMode = TIM_ENCODERMODE_TI12;
 sConfig.IC1Polarity = TIM_ICPOLARITY_RISING;
 sConfig.IC1Selection = TIM_ICSELECTION_DIRECTTI;
 sConfig.IC1Prescaler = TIM_ICPSC_DIV1;
 sConfig.IC1Filter = 10;
 sConfig.IC2Polarity = TIM_ICPOLARITY_RISING;
 sConfig.IC2Selection = TIM_ICSELECTION_DIRECTTI;
 sConfig.IC2Prescaler = TIM_ICPSC_DIV1;
 sConfig.IC2Filter = 5;
 if (HAL_TIM_Encoder_Init(&htim3, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM3_Init 2 */

 /* USER CODE END TIM3_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_13, GPIO_PIN_RESET);

 /*Configure GPIO pin : PC13 */
 GPIO_InitStruct.Pin = GPIO_PIN_13;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * file: pointer to the source file name
 * line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

This topic has been closed for replies.

8 replies

Andrew Neil
Super User
Feb 28, 2024 12:06 PM UTC

Please use this button to properly post source code:

AndrewNeil_0-1709121700169.png

 


@ahmetefek12 wrote:

My project is reading encoder data, and then send this data to the terminal via USB connection */


An encoder just gives a stream of pulses - how do you envisage sending this as "data" to a terminal?

 


@ahmetefek12 wrote:

I cannot see the encoder data in the terminal. 


Do one step at a time: before worrying about all the encoder stuff, can you just send a fixed, "hello, world" string over the CDC ?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
Feb 28, 2024 12:48 PM UTC

Sorry for the misuse, I'm new to the community.

I am using TIMER encoder mode to read encoder data. I expect to receive data between 0-65535 depending on the encoder position.

And yes, I can see the string message in the terminal like "hello pc". But when I want to see an integer value, I cannot see it in the terminal.

By the way, I think I need to enter an ASCII value into the function. Because when I set my variable equal to 48, I see the decimal number 0 in the terminal. But I'm still not sure about how to handle encoder data.

Andrew Neil
Super User
Feb 28, 2024 1:02 PM UTC

@ahmetefek12 wrote:

I can see the string message in the terminal like "hello pc". But when I want to see an integer value, I cannot see it in the terminal.

By the way, I think I need to enter an ASCII value into the function. Because when I set my variable equal to 48, I see the decimal number 0 in the terminal. But I'm still not sure about how to handle encoder data.


Again, take it one step at a time.

Get the sending of simple integer data working before adding all the encoder stuff.

Yes, if you're sending data to a terminal it will have to be as human-readable text.

C has library functions for converting numbers to text; eg, sprintf(), itoa()

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ST Technical Moderator
Mar 5, 2024 4:43 PM UTC

Hi @ahmetefek12 

Would you please specify the target used? your environment including (toolchain, cube firmware used etc..)?

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Associate II
Mar 6, 2024 9:46 AM UTC

STM32CubeIDE for programming, ST-Link utility for debugging (i'm uploading hex file to stm32) and Hercules as terminal. My encoder is incremental magnetic (am-3479) but project is for any kind of incremental encoder.

ST Technical Moderator
Mar 6, 2024 10:51 AM UTC

I suggest starting with using sprintf or a similar function that can simplify the process of converting the encoder value to a string of ASCII characters. The function takes care of the conversion and formatting for you, so you don't have to worry about manually converting each digit to ASCII and storing each digit in an array.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL