Question
'register' specifier in Cube/LL
I have a bunch of following warnings:
c:/programs/ARMtools/EmbeddedBSPs/arm-eabi/com.sysprogs.arm.stm32/STM32F1xxxx/STM32F1xx_HAL_Driver/Inc/stm32f1xx_ll_gpio.h: In function 'void LL_GPIO_SetPinMode(GPIO_TypeDef*, uint32_t, uint32_t)':
c:/programs/ARMtools/EmbeddedBSPs/arm-eabi/com.sysprogs.arm.stm32/STM32F1xxxx/STM32F1xx_HAL_Driver/Inc/stm32f1xx_ll_gpio.h:343:22: warning: ISO C++17 does not allow 'register' storage class specifier [-Wregister]
343 | register uint32_t *pReg = (uint32_t *)((uint32_t)((uint32_t)(&GPIOx->CRL) + (Pin >> 24)));
|in several LL headers.
Can this please be fixed in some suitable way? One way to do that might be to replace the 'register' specifier by a macro, which would be defined based on the __cplusplus standard preprocessor macro and its value. A simple version would be to add
#if __cplusplus >= 201703L
#define register
#endifto each header where this occurs, but I am not a C++/build-environment specialist so don't know whether this may have some unwanted effect I am not aware off.
Thanks,
JW