Question
problem in connecting dfuse with STM32 board using USB
Posted on June 11, 2013 at 12:05
Hi,
I have downloaded Dfuse and using the external Boot pins i jumped into the bootloader area(system memory), but dfuse is not detecting my device..when i connect the USB it shows as unknown device at the device manager but as mentioned in the dfuse document i installed the driver , now i can see the '' stm32 device in dfu mode '' at device manager with an error code10(cannot the start the device). my system is 64 bit operating system.. 1. pls suggest me any ideas of how to do it.?2. Is there any other Application available to reprogram the device using boot loader ? #dfu-dfuse-bootloader #usb #!sms