2021-12-23 12:56 AM
Hello!
I have an STM32F769I-DISCO board and I would like to power it by using the USB HS connector. I have just found that power bank 57960 P/PACK RS | Varta 6Ah 5V Power Bank Portable Charger | RS Components (rs-online.com) and I am wondering whether I really can use it (especially the 5V/1A output) to power my board with no risk of breaking.
Thank you very much in advance for your help!
Solved! Go to Solution.
2021-12-23 2:28 AM
Normally the power banks generate a voltage of 5V, which is in the normal USB range, so that you can also use them for the supply via USB HS.
Please don't forget to move the jumper on CN3 from ST_LINK to USB_HS.
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2021-12-23 2:28 AM
Normally the power banks generate a voltage of 5V, which is in the normal USB range, so that you can also use them for the supply via USB HS.
Please don't forget to move the jumper on CN3 from ST_LINK to USB_HS.
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2021-12-23 2:46 AM
Of course, thank you very much for your quick reply!