Skip to main content
Associate II
October 3, 2024
Question

NUCLEO-F446RE SMARTMIC1 with MP34DT06J Microphone

  • October 3, 2024
  • 1 reply
  • 667 views

Hardware:

NUCLEO-F446RE,  X-NUCLEO-CCA01M1,  X-NUCLEO-CCA02M2

Software: 

SMARTMIC1 V2.4.0 & V2.3.0

 

I am attempting to run the SMARTMIC1 program on the hardware list above but instead of using the microphones on the  STEVAL-MIC001V1, I want to use the CCA02M2 onboard MP34DT06J microphones. 

In an attempt to achieve this on CCA02M2 I changed the position of J2 to position 1-2, removed J3, and installed the solder bridge on SB9.

While Audacity will start recording, 0 microphone volume is recorded. 

I am now looking into the cca02m2_conf.h file and change the AUDIO_IN_CHANNELS from 4 to 2. 

In Audacity, channel 2 is 100% volume, and channel 1 is 0% volume. 

Is there any way to achieve what I am trying to do? 

This topic has been closed for replies.

1 reply

SimonePradolini
ST Technical Moderator
October 15, 2024

Hello @OceanPlumber 

The SMARTMIC1 demo is meant to work with 4 microphones only. Updating the cca02m2_conf.h file is not sufficient.

The demo uses a custom USB class that allows both USB audio communication and serial communication so that the firmware can be controlled by the GUI distributed in the package. It is a complex setup, designed to showcase the Acoustic libraries at their maximum capacity.

If you'd like to focus your attention on easier examples, I suggest you look into X-CUBE-MEMSMIC1, where you can find a specific example for any of the audio in related Acoustic library. Natively, it supports NUCLEO-F401RE, but porting it to NUCLEO-F446RE is straightforward (both Nucleo boards use the same Cortex).

 

Best regards,
Simone

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.