Skip to main content
Associate III
Dec 18, 2024 12:10 PM UTC
Solved

Non Blocking programming

I have a STM32F411 board connected with a GPS module connected onto USART2
I also have Tim1 and Tim3 configured for PWM generation on their channels respectively.

I am running a list of commands (from an array) to execute line for line.

Most of the execution is in the form of assigning new values to the Timer channels

Eg: __HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_2, motor1_speed); Motor speed is a variable assigned from the list. As the program executes the list (by iterating  line for line, these variables get assigned those values.)

The GPS on the other hand is being polled via USART2

The problem is that I need both the execution of the array as well as the GPS to continue running.

However, the array execution is causing a "blocking issue". I have about 15 lines of instructions in the executing array. The GPS will only work AFTER ALL the commands of the array has been executed due to its blocking issue.

I investigated from many sources who advised:

  1. Use RTOS - this did not work. It still blocks
  2. Use another Timer to run the GPS. - Still did not work.

Any assistance here?

This topic has been closed for replies.
Andrew Neil
Andrew NeilBest answer
Super User
Dec 18, 2024 3:43 PM UTC

@techdesk wrote:

As the execution iterates (after the time in seconds) it assigns the values to motor2 and motor3 respectively. 
That said, these executing lines are blocking the GPS


That doesn't make sense:  those __HAL_TIM_SET_COMPARE are simply writing a value to a register - the time for which they "block" is minuscule.

Or are you saying you do that continuously in a tight loop?

 


@techdesk wrote:

Here is the code:

 

#define UART_QUEUE_SIZE 64 QueueHandle_t uartQueue;

void GPS_Task(void *pvParameters) { uint8_t received_byte; while (1) { // Wait for a byte from the queue if (xQueueReceive(uartQueue, &received_byte, portMAX_DELAY) == pdPASS) { // Process the byte processGPSData(&received_byte, 1); } } }

void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) { if (huart->Instance == USART2) { // Send received byte to the queue xQueueSendFromISR(uartQueue, &received_char, NULL); // Re-enable UART interrupt for next byte HAL_UART_Receive_IT(&huart2, &received_char, 1); } }
In the HAL_UART_RxCpltCallback() I have this:
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) { if (huart->Instance == USART2) { // Send received byte to the queue xQueueSendFromISR(uartQueue, &received_char, NULL); // Re-enable UART interrupt for next byte HAL_UART_Receive_IT(&huart2, &received_char, 1); } }

 


Please would you re-post that - each function seems to have got compressed onto a single line!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

23 replies

TDK
Dec 18, 2024 1:13 PM UTC

There is no reason you can't have these in two different tasks in FreeRTOS.

Note that only one thread can run at a time, it will switch back and forth between them at a relatively fast rate.

> However, the array execution is causing a "blocking issue".

Too vague. Step through the code. What is happening? What do you expect to happen instead?

"If you feel a post has answered your question, please click ""Accept as Solution""."
techdeskAuthor
Associate III
Dec 18, 2024 1:52 PM UTC

Ok, firstly the answer to your question:
"Too vague. Step through the code. What is happening? What do you expect to happen instead?"
Here is the array:

MotorInstruction instructions[] = {

{'F', {900, 900}, 10}, // Move forward at speed 900 for 10 seconds

{'F', {100, 600}, 3}, // Turn with speeds 500 and 600 for 3 seconds

{'F', {600, 600}, 10}, // Move forward at speed 600 for 10 seconds

{'F', {700, 700}, 3},// Move forward at speed 1000 for 3 seconds

{'F', {900, 900}, 3},

// etc etc.....

};

These figures are assigned to the respective timer channels 
eg: 

__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_2, motor2_speed);
__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_3, motor3_speed);


As the execution iterates (after the time in seconds) it assigns the values to motor2 and motor3 respectively. 
That said, these executing lines are blocking the GPS which is automatically coming through the USART2.
You mention RTOS.
I spent hours with the RTOS task. Maybe I was not doing things correctly.

Here is the code:

#define UART_QUEUE_SIZE 64 QueueHandle_t uartQueue;

void GPS_Task(void *pvParameters) { uint8_t received_byte; while (1) { // Wait for a byte from the queue if (xQueueReceive(uartQueue, &received_byte, portMAX_DELAY) == pdPASS) { // Process the byte processGPSData(&received_byte, 1); } } }

void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) { if (huart->Instance == USART2) { // Send received byte to the queue xQueueSendFromISR(uartQueue, &received_char, NULL); // Re-enable UART interrupt for next byte HAL_UART_Receive_IT(&huart2, &received_char, 1); } }
In the HAL_UART_RxCpltCallback() I have this:
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) { if (huart->Instance == USART2) { // Send received byte to the queue xQueueSendFromISR(uartQueue, &received_char, NULL); // Re-enable UART interrupt for next byte HAL_UART_Receive_IT(&huart2, &received_char, 1); } }

Then in my INT Main
I have this:

 // Initialize the FreeRTOS queue
 uartQueue = xQueueCreate(UART_QUEUE_SIZE, sizeof(uint8_t));
 if (uartQueue == NULL) {
 // Handle queue creation error
 Error_Handler(); }
 // Create the GPS task
 xTaskCreate(GPS_Task, "GPS_Task", 128, NULL, 2, NULL); // Stack size = 128, priority = 2
 // Start the scheduler
 vTaskStartScheduler();

Like I said, this code ought to work. But nothing happens

TDK
Dec 18, 2024 2:48 PM UTC

The __HAL_TIM_SET_COMPARE statements do not block. Must be some other reason.

In your FreeRTOS code, you're only creating a task for the GPS. You should have another task for the motor control, if you want them to run concurrently.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Tesla DeLorean
Guru
Dec 18, 2024 3:58 PM UTC

What exactly is "not working"?

What exactly is "blocking" here?

Break the problem down, is the GPS reading and parsing successfully?

This type of one byte queuing is going to be very burdensome. Perhaps make a bigger buffer you fill in the interrupt handler, QUICKLY,  and the process the buffer as you have occasion to do some, perhaps after you've done the super-critical stuff. Parsing shouldn't take a lot of time, unless you hang it up with other output, or code that spins to accomodately slower processes.

What you've described to this point could be done with very light weight code, with some time critical stuff handled in interrupts, and others is a main loop. General rule would be to do stuff you can, don't stall, come back and check later.

Most difficult thing for most people to break free of is linear code execution, and simply move it to multiple threads enforcing similar knock-on dependencies and sequencing.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
techdeskAuthor
Associate III
Dec 18, 2024 4:08 PM UTC

I accidentally pressed the "accepted".  Sorry
Any case, I am still trying to work around RTOS. 
Regarding the GPS, I have reverted to buffer mode. So I get bigger chunks.
Look, the GPS function WORKS 100%. But like I said the execution of the Array is blocking it. Until the array is finished, the gps shows again. RTOS in my opinion is maybe for lrager processors. Boards like the STMF411 may not be suitable. Also, the RTOS works. but execution is SLOW. Very Slow. 10 seconds turn into almost 60 seconds 
Anycase, I will just battle on. I will retry and juggle between the USART DMA etc. I will find some solution. And belive me I have tried abundantly. 
Many responders to this thread give advice, but no sample code to test. Best not to respond rather than give fresh air code 


Andrew Neil
Super User
Dec 18, 2024 6:04 PM UTC

@Andrew Neil wrote:

You could use the same principle as here:

https://docs.arduino.cc/built-in-examples/digital/BlinkWithoutDelay/

HAL_GetTick() is equivalent to the Arduino millis() ...


Here you go - blinking two LEDs with unrelated periods:

 

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */

 uint32_t ld4_blu_interval = 2000;
 uint32_t ld3_grn_interval = 3000;

 uint32_t ld4_blu_previous_tick = 0;
 uint32_t ld3_grn_previous_tick = 0;

 while (1)
 {
	 uint32_t current_tick = HAL_GetTick();

	 if( current_tick - ld4_blu_previous_tick >= ld4_blu_interval )
	 {
		 ld4_blu_previous_tick = current_tick;
		 HAL_GPIO_TogglePin( ld4_blu_GPIO_Port, ld4_blu_Pin );
	 }

	 if( current_tick - ld3_grn_previous_tick >= ld3_grn_interval )
	 {
		 ld3_grn_previous_tick = current_tick;
		 HAL_GPIO_TogglePin( ld3_grn_GPIO_Port, ld3_grn_Pin );
	 }

 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

 

(Tested on an F0-DISCOVERY board, with User LEDs LD3 Green and LD4 Blue)

I've just duplicated everything for the 2 LEDs there; more generally, it'd be better to factor that into a function (or functions) ...

 

#NonBlockingDelay #NonBlockingBlinky #NoDelayBlinky

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
techdeskAuthor
Associate III
Dec 18, 2024 8:15 PM UTC

Like I said, I finally manged to:
1. Read GPS via USART2,
2. Send/Receive text commands via USART1.
3. Execute a list of commands in the Main()
ALL simultaneously!
I. I enabled Interrupts for both USARTs
2. added this also in the Main() (just an example of my code)

HAL_UART_Receive_IT(&huart1, (uint8_t *)&received_char, 1);

HAL_UART_Receive_IT(&huart2, (uint8_t *)&received_char, 1);
Without these lines in the Main(), it will NEVER work
This is a super feat especially for projects requiring autonomous mode.
If anyone needs further details, I will provide.
In any case, thank you all for your helping attempts

Karl Yamashita
Principal
Dec 18, 2024 9:04 PM UTC

@techdesk wrote:

Like I said, I finally manged to:
1. Read GPS via USART2,
2. Send/Receive text commands via USART1.
3. Execute a list of commands in the Main()
ALL simultaneously!
I. I enabled Interrupts for both USARTs
2. added this also in the Main() (just an example of my code)

HAL_UART_Receive_IT(&huart1, (uint8_t *)&received_char, 1);

HAL_UART_Receive_IT(&huart2, (uint8_t *)&received_char, 1);
Without these lines in the Main(), it will NEVER work
This is a super feat especially for projects requiring autonomous mode.
If anyone needs further details, I will provide.
In any case, thank you all for your helping attempts


You say you added HAL_UART_Receive_IT to main. But you don't say where in main. 

Show MORE of your complete code so we can see the bigger picture, not just snippets

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source