Skip to main content
Associate II
Jun 2, 2025 6:45 AM UTC
Question

+ connecting to PC as a audio device class

Hello, 

I am developing STM audio streaming device by nucleo-H753ZI.

 

Just I have done is bellow like:

1. configure  HSE by Cube MX and applied 25 MHz external oscillator physically .

- It works well when USB OTG FS mode.

2. Physically connected between H753ZI and  USB3300 ULPI 

(D0~D7, 3.3Vs, GNDs, NXT, DIR, RST, STP,  CLK)

D0->PA3,

D1->PB0,

D2-> PB1,

D3->PB10,

D4->PB11,

D5->PB12,

D6->PB13,

D7->PB5,

STP->PC0,

NXT->PC3,

DIR->PC2,

CLK->PA5,

2 of 3.3V pins,

2 of GND pins 

 

3. Checked Cube MX options : 

- USB OTG FS : Disabled

- USB OTG HS - Device only

- USB Device - (Class for HS IP) Audio Device Class, 48000 sample/s, Device descriptor : 1200

- NVIC : priority

    USB OTG global interrupt = 0
    USB OTG EndPoint I/O global interrupt = 0

4. Connected to PC as USB : No device detected on PC!

( I have edit MX_USB_DEVICE_Init(void) function for debugging : 

/* USER CODE BEGIN USB_DEVICE_Init_PostTreatment */
HAL_Delay(10); //insert
HAL_PWREx_EnableUSBVoltageDetector();

/* USER CODE END USB_DEVICE_Init_PostTreatment */

)

 

I wonder I have missed something essential...

could you let me know it?
Thank you.

 

This topic has been closed for replies.

3 replies

ST Technical Moderator
Jun 2, 2025 1:00 PM UTC

Hi @skson 

First, I recommend using CRS SYNC with USB HS instance. This can be configured in CubeMX under the RCC tab.

Second, noticed the addition of HAL_Delay(10);. Could you clarify the purpose of this delay?

For your firmware configuration, I suggest referring to the example provided under ./Projects/STM32H747I-EVAL/Applications/USB_Device/Audio_Standalone

When using an external circuit for the ULPI interface, it’s crucial to ensure proper routing for signal integrity. Double-check for any loose connections or soldering issues. Consider using a logic analyzer or oscilloscope to monitor the ULPI signals.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
sksonAuthor
Associate II
Jun 4, 2025 1:21 AM UTC

Dear, 

I'm appreciate your fast response.

1. Just following your advice, I enabled CRS SYNC with USB HS instance but there is no changes...

2. additional code : HAL_Delay(10); If it does not added, the code is stopped while running MX_USB_DEVICE_Init(). While debugging, it is result of trials, to avoid the runtime error.

I don't know why, but added this delay, it passed well.

3. I understand your wording as : there is an example of H7 USB Device - USB OTG HS Audio class.

If you share it correctly, it might help.

But I cannot find "Audio_Standalone" example in ./Projects/STM32H747I-EVAL/Applications/USB_Device/ folder.

To me, it seems like under : 

skson_1-1748998202450.png

Best regards,

From Son.

 

ST Technical Moderator
Jun 4, 2025 10:49 AM UTC

Hi again @skson 

Some middleware libraries along with the projects are not available on Github. You can find them directly when downloading from STM32CubeH7.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL