Skip to main content
Visitor II
October 24, 2024
Question

ll_usb in STM32H7RS hal driver uses a Reserved setting of OTG_GAHBCFG.HBSTLEN

  • October 24, 2024
  • 1 reply
  • 576 views

https://github.com/STMicroelectronics/stm32h7rsxx-hal-driver/blob/ecc746788b9843dd4295f0acb58b3d15c3477abb/Src/stm32h7rsxx_ll_usb.c

In stm32h7rsxx_ll_usb.c in function USB_CoreInit:

if (USBx == USB_OTG_HS)
{
if (cfg.phy_itface == USB_OTG_HS_EMBEDDED_PHY)
{
/* Init The UTMI Interface */
USBx->GUSBCFG &= ~(USB_OTG_GUSBCFG_TSDPS);
}

/* Reset after a PHY select */
ret = USB_CoreReset(USBx);

if (cfg.dma_enable == 1U)
{
USBx->GAHBCFG |= USB_OTG_GAHBCFG_HBSTLEN_2;
USBx->GAHBCFG |= USB_OTG_GAHBCFG_DMAEN;
}
}

It set USB_OTG_GAHBCFG_HBSTLEN_2 in GAHBCFG, so GAHBCFG.HBSTLEN should be 0b0100.

But in RM0477(Reference Manual for STM32H7RS):

Bits 4:1 HBSTLEN[3:0]: Burst length/type

0000 Single: Bus transactions use single 32 bit accesses (not recommended)

0001 INCR: Bus transactions use unspecified length accesses (not recommended, uses the

INCR AHB bus command)

0011 INCR4: Bus transactions target 4x 32 bit accesses

0101 INCR8: Bus transactions target 8x 32 bit accesses

0111 INCR16: Bus transactions based on 16x 32 bit accesses

Others: Reserved

 

But 0b0100 for HBSTLEN is Reserved. So the code is correct or the RM0477 is correct?

This topic has been closed for replies.

1 reply

ST Technical Moderator
January 8, 2025

Hi @VSF 

Thank you for reporting this incoherency, an internal ticket (199817) is submitted to dedicated team. 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL