2024-12-17 1:27 AM
Hello Everyone,
I am working on a UVC project using the STM32U5G9ZJT6Q MCU, capturing 8-bit data via DCMI and streaming it over USB UVC to VLC or Windows Camera. To achieve higher FPS, I need to increase the USBD_VIDEO_EPIN_HS_MPS (High-Speed Max Packet Size) above 2500.
However, when I try to set USBD_VIDEO_EPIN_HS_MPS beyond 2000, the image does not display, and no data appears in Wireshark.
Is there a way to increase USBD_VIDEO_EPIN_HS_MPS above 2500 reliably, or are there specific configurations needed to support higher packet sizes?
Any guidance or insights would be greatly appreciated.
Thank you in advance!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.