Skip to main content
MMerc.1
Associate III
November 19, 2020
Solved

How can I update the software on STM32F7 ?

  • November 19, 2020
  • 11 replies
  • 3488 views

Hi,

I want to update the software of the STM32F746BGT via a USB stick or Ethernet connexion.

Firstly, how can I use the USB stick to update the software inside the MCU ?

How can I use the Internet connexion (via UART : Lantronix XPORT) to update the software inside the MCU ?

Best regards

This topic has been closed for replies.
Best answer by KnarfB

Partition your code into a bootloader and the real application. The bootloader normally just starts the real app. When some condition is set to true, the bootloader instead communicates with the peripheral(s), downloads + flashes a new version of the app into the flash and finally reboots.

11 replies

KnarfB
KnarfBBest answer
Super User
November 19, 2020

Partition your code into a bootloader and the real application. The bootloader normally just starts the real app. When some condition is set to true, the bootloader instead communicates with the peripheral(s), downloads + flashes a new version of the app into the flash and finally reboots.

MMerc.1
MMerc.1Author
Associate III
November 23, 2020

Hi,

Do you think the example of "STM32Cube_FW_F7_V1.16.0\Projects\STM32756G_EVAL\Applications\USB_Host\FWupgrade_Standalone" works ?

MMerc.1
MMerc.1Author
Associate III
December 1, 2020

Hi,

I try to use the example of "STM32Cube_FW_F7_V1.16.0\Projects\STM32756G_EVAL\Applications\USB_Host\FWupgrade_Standalone" but when I add "#include <usbh_def.h>" in order to use the structure for "extern USBH_HandleTypeDef hUsbHostFS" in main.h I have the following error :

make -j12 all 
arm-none-eabi-gcc "../USB_HOST/Target/usbh_conf.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32F746xx -DDEBUG -c -I../TouchGFX/gui/include -IC:/Users/ozone/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -I../USB_HOST/App -I../TouchGFX/generated/fonts/include -IC:/Users/ozone/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Middlewares/Third_Party/FreeRTOS/Source/include -IC:/Users/ozone/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Middlewares/Third_Party/FatFs/src -I../TouchGFX/generated/texts/include -I../TouchGFX/generated/images/include -IC:/Users/ozone/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1 -I"C:/Users/ozone/STM32CubeIDE/workspace_1.3.0/OZONEX_IHM_208/Components/ft5336" -IC:/Users/Stef/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -IC:/Users/Stef/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Inc -IC:/Users/ozone/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Middlewares/ST/STM32_USB_Host_Library/Core/Inc -I../Core/Inc -IC:/Users/ozone/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Drivers/CMSIS/Include -I../TouchGFX/generated/gui_generated/include -IC:/Users/ozone/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS -IC:/Users/ozone/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Drivers/STM32F7xx_HAL_Driver/Inc -I../FATFS/App -I"C:/Users/ozone/STM32CubeIDE/workspace_1.3.0/OZONEX_IHM_208/Components/Common" -IC:/Users/ozone/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Drivers/CMSIS/Device/ST/STM32F7xx/Include -IC:/Users/Stef/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Drivers/CMSIS/Device/ST/STM32F7xx/Include -I"C:/Users/ozone/STM32CubeIDE/workspace_1.3.0/OZONEX_IHM_208/STM32746G-Discovery" -IC:/Users/Stef/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Middlewares/Third_Party/FatFs/src -IC:/Users/ozone/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Inc -I../Middlewares/ST/touchgfx/framework/include -IC:/Users/Stef/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1 -IC:/Users/Stef/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Middlewares/Third_Party/FreeRTOS/Source/include -I../TouchGFX/target/generated -IC:/Users/Stef/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Middlewares/ST/STM32_USB_Host_Library/Core/Inc -IC:/Users/Stef/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Drivers/STM32F7xx_HAL_Driver/Inc -I../FATFS/Target -I../TouchGFX/App -IC:/Users/Stef/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS -I../USB_HOST/Target -I../TouchGFX/target -IC:/Users/Stef/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"USB_HOST/Target/usbh_conf.d" -MT"USB_HOST/Target/usbh_conf.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "USB_HOST/Target/usbh_conf.o"
In file included from ../Core/Inc/main.h:38:0,
 from ../USB_HOST/Target/usbh_conf.h:33,
 from C:/Users/ozone/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Middlewares/ST/STM32_USB_Host_Library/Core/Inc/usbh_core.h:28,
 from ../USB_HOST/Target/usbh_conf.c:23:
C:/Users/ozone/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Middlewares/ST/STM32_USB_Host_Library/Core/Inc/usbh_def.h:280:44: error: 'USBH_MAX_NUM_ENDPOINTS' undeclared here (not in a function); did you mean 'USB_DESC_ENDPOINT'?
 USBH_EpDescTypeDef Ep_Desc[USBH_MAX_NUM_ENDPOINTS];
 ^~~~~~~~~~~~~~~~~~~~~~
 USB_DESC_ENDPOINT
C:/Users/ozone/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Middlewares/ST/STM32_USB_Host_Library/Core/Inc/usbh_def.h:295:45: error: 'USBH_MAX_NUM_INTERFACES' undeclared here (not in a function); did you mean 'USBH_MAX_NUM_ENDPOINTS'?
 USBH_InterfaceDescTypeDef Itf_Desc[USBH_MAX_NUM_INTERFACES];
 ^~~~~~~~~~~~~~~~~~~~~~~
 USBH_MAX_NUM_ENDPOINTS
C:/Users/ozone/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Middlewares/ST/STM32_USB_Host_Library/Core/Inc/usbh_def.h:422:49: error: 'USBH_MAX_SIZE_CONFIGURATION' undeclared here (not in a function); did you mean 'USB_REQ_SET_CONFIGURATION'?
 uint8_t CfgDesc_Raw[USBH_MAX_SIZE_CONFIGURATION];
 ^~~~~~~~~~~~~~~~~~~~~~~~~~~
 USB_REQ_SET_CONFIGURATION
C:/Users/ozone/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Middlewares/ST/STM32_USB_Host_Library/Core/Inc/usbh_def.h:423:42: error: 'USBH_MAX_DATA_BUFFER' undeclared here (not in a function); did you mean 'USBH_MAX_PIPES_NBR'?
 uint8_t Data[USBH_MAX_DATA_BUFFER];
 ^~~~~~~~~~~~~~~~~~~~
 USBH_MAX_PIPES_NBR
C:/Users/ozone/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Middlewares/ST/STM32_USB_Host_Library/Core/Inc/usbh_def.h:460:32: error: 'USBH_MAX_NUM_SUPPORTED_CLASS' undeclared here (not in a function); did you mean 'USBH_NOT_SUPPORTED'?
 USBH_ClassTypeDef *pClass[USBH_MAX_NUM_SUPPORTED_CLASS];
 ^~~~~~~~~~~~~~~~~~~~~~~~~~~~
 USBH_NOT_SUPPORTED
make: *** [USB_HOST/Target/subdir.mk:18: USB_HOST/Target/usbh_conf.o] Error 1
"make -j12 all" terminated with exit code 2. Build might be incomplete.
 
09:16:05 Build Failed. 6 errors, 0 warnings. (took 13s.12ms)

Do you have any idea about this error ?

Best regards

Frak.1
Associate II
December 1, 2020

For me it is too less information. Can you share your project or this library? How this variables are declared? For example "USBH_MAX_NUM_ENDPOINTS". Are they as #define? Looks like the compiler can't find their declarations.

MMerc.1
MMerc.1Author
Associate III
December 1, 2020

Hi,

I fixed the error. But now, I am trying to figure out how it works.

I call the function "HCD_Port_IRQHandler" and I have to call the function "HAL_HCD_PortEnabled_Callback". Unfortunately, the variable "hprt0" does not have a "USB_OTG_HPRT_PENA" bit... So function "HAL_HCD_PortEnabled_Callback" is never called.

Do you know why ?

Edit 1 :

I fixed the error. Now in case "HOST_CHECK_CLASS" in the function "USBH_Process", I don't have "USBH_OK" when I use "phost->pActiveClass->Init(phost)".

Do you know why ?

Edit 2 :

The problem is in the function "static USBH_StatusTypeDef USBH_MSC_InterfaceInit(USBH_HandleTypeDef *phost)" :

phost->pActiveClass->pData = (MSC_HandleTypeDef *)USBH_malloc(sizeof(MSC_HandleTypeDef));
 MSC_Handle = (MSC_HandleTypeDef *) phost->pActiveClass->pData;

MSC_Handle return NULL value.

Frak.1
Associate II
December 1, 2020

From this little part of the code I conclude that USBH_malloc can't allocate memory. Malloc returns NULL when it can't allocate enough space.