Skip to main content
Divyanshu
Associate II
April 6, 2021
Question

ECHO_TCP_Server (LWIP)

  • April 6, 2021
  • 2 replies
  • 930 views

TCP_ECHO_Server

When I open TCP port and send some data on that port. It works fine.

But if I open 2 tcp port at same IP and same port (Max port I can have 5) .So while receiving data on both i gets the data alternatively on each port.

I want data should travel on each port irrespective of the number. Because port is same.

This topic has been closed for replies.

2 replies

Vangelis Fortounas
Associate II
April 7, 2021

Hello

>> I want data should travel on each port irrespective of the number. Because port is same.

I am not sure that lwip programmers took care about this special case to listen to two times the same port.

if packet is for x.x.x.x IP and y Port, what is the meaning to process the same packet 2 times?

Note that after processing an input buffer the processing callback frees the buffer so can't be processed second time.

Divyanshu
DivyanshuAuthor
Associate II
May 20, 2021

Hi Vangelis

Sorry, I was not active for long time.

With respect to above issue, if packet is for x.x.x.x IP and y Port and let say packet is "abc".

I opened a tcp client on my laptop with x.x.x.x IP and y Port( Terminal-1). and i opened another terminal with same x.x.x.x IP and y Port.(called terminal-2)

Now when I send data "abc", I will receive"123" in return from my devices. So i receive "123" from my devices but it comes alternatively ( first on terminal-1 then on terminal 2).But it should come to both terminal simultaneously irrespective of the terminal.

Just like Wireshark software does.