Skip to main content
Associate II
January 9, 2025
Question

Does HAL_FLASH_OB_Launch cause a system reset on STM32H563 MCU?

  • January 9, 2025
  • 1 reply
  • 1749 views
As for STM32H563 MCU, will it result in a system reset after executing the function HAL_FLASH_OB_Launch?
 
From my experiment, before executing HAL_FLASH_OB_Launch, I can read data from MCU via I2C while all returned data become 0xFF(i.e. invalid data) after executing this function.
 
It seems that the MCU is suspended or reset. When I tried to trace the code through Debugger Section in Keil, the code can run smoothly to subsequent routines.
 
Here is my code below.
 

 

 

void EnableWriteProtect(uint8_t image)
{
 FLASH_OBProgramInitTypeDef OBInit = {0};
 FLASH_OBProgramInitTypeDef sOBPrev = {0};

 uint32_t WRPSector;

 /* Unlock the User Flash area */
 HAL_FLASH_Unlock();
 HAL_FLASH_OB_Unlock();

 /* Get the boot configuration status */
 HAL_FLASHEx_OBGetConfig(&OBInit);

 WRPSector = OBInit.WRPSector | BIT(0);

 OBInit.Banks = FLASH_BANK_2;
 OBInit.OptionType = OPTIONBYTE_WRP;
 OBInit.WRPState = OB_WRPSTATE_ENABLE;
 OBInit.WRPSector = WRPSector;
 HAL_FLASHEx_OBProgram(&OBInit);

 /* Launch Option bytes loading */
 HAL_FLASH_OB_Launch();

 /* Unlock the User Flash area */
 HAL_FLASH_Lock();
 HAL_FLASH_OB_Lock();
}

 

 

 
My expectation: I hope to implement write protection for specific MCU flash areas normally without resetting the MCU.

1 reply

TDK
January 9, 2025

> Does HAL_FLASH_OB_Launch cause a system reset on STM32H563 MCU?

No, HAL_FLASH_OB_Launch sets FLASH_OPTCR_OPTSTART which reloads the option bytes but does not reset the chip.

 

The typical way of modifying option bytes is to only change them if needed. If WRP is already set correctly, no need to modify them.

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
XeManAuthor
Associate II
January 17, 2025

Reference manual section 7.4.3 says that user should reset the device after changing option bytes. This is mandatory under certain circumstances, strongly recommend otherwise.

So I think I should follow the rule to perform "device reset" after programming flash option byte.

user manualuser manual