Skip to main content
Associate II
Mar 25, 2024 1:59 PM UTC
Solved

Array for GPIO pins

Hello,

 

I am new to STM world.

I am trying to make an array of GPIO pin in this format {{PIN1_GPIO_PORT, PIN1_PIN}.....

This would then be used in custom function so I can dynamically access this pins.

How should I declare such array and how would i use them with HAL_GPIO_WRITEPIN function.

Main use of this is to select SPI slave to communicate with.

 

Thanks in advance

 

This topic has been closed for replies.
Andrew Neil
Andrew NeilBest answer
Super User
Mar 25, 2024 2:14 PM UTC

@Huzo wrote:

I am new to STM world.


Do you have any experience with any other microcontrollers?

Do you have any experience with programming in general? With C programming?

 


@Huzo wrote:

I am trying to make an array of GPIO pin in this format {{PIN1_GPIO_PORT, PIN1_PIN}.....


I would have a struct for the {port,pin} pair, and then make an array of those structs ...

As you want to use it with HAL_GPIO_WritePin, make the types compatible with what that function requires:

void HAL_GPIO_WritePin(GPIO_TypeDef* GPIOx, uint16_t GPIO_Pin, GPIO_PinState PinState)

 

So you'd have something like

typedef struct 
{
 GPIO_TypeDef* GPIOx;
 uint16_t GPIO_Pin;
} port_and_pin_t;

port_and_pin_t ports_and_pins[length];

:
:

HAL_GPIO_WritePin( ports_and_pins[x].GPIOx, ports_and_pins[x].GPIO_Pin, value );

 

You might want to make a "wrapper" function which just takes the struct, breaks-out the 2 elements, and passes them to HAL_GPIO_WritePin ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

16 replies

gbm
Super User
Mar 25, 2024 2:07 PM UTC

<deleted - the right answer was posted below>

 

struct pin_ {
    GPIO_TypeDef *port;
    uint16_t pinmask;
};

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
Andrew Neil
Super User
Mar 25, 2024 2:30 PM UTC

@gbm wrote:

<deleted - the right answer was posted below>


For one thing, I think your choice of "pinmask" as the name for the pin element is better than mine!

I always find the ST documentation very unclear on whether these HAL functions expect a pin mask or a pin number.

:frowning_face:

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
HuzoAuthor
Associate II
Mar 25, 2024 2:33 PM UTC

There is no perfect documentation. I will try to make the structure and use without my function, for testing purposes, and will come here with a reply. Thanks.

Tesla DeLorean
Guru
Mar 25, 2024 2:11 PM UTC

Create a structure, array the structure. More C than STM32

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Andrew NeilBest answer
Super User
Mar 25, 2024 2:14 PM UTC

@Huzo wrote:

I am new to STM world.


Do you have any experience with any other microcontrollers?

Do you have any experience with programming in general? With C programming?

 


@Huzo wrote:

I am trying to make an array of GPIO pin in this format {{PIN1_GPIO_PORT, PIN1_PIN}.....


I would have a struct for the {port,pin} pair, and then make an array of those structs ...

As you want to use it with HAL_GPIO_WritePin, make the types compatible with what that function requires:

void HAL_GPIO_WritePin(GPIO_TypeDef* GPIOx, uint16_t GPIO_Pin, GPIO_PinState PinState)

 

So you'd have something like

typedef struct 
{
 GPIO_TypeDef* GPIOx;
 uint16_t GPIO_Pin;
} port_and_pin_t;

port_and_pin_t ports_and_pins[length];

:
:

HAL_GPIO_WritePin( ports_and_pins[x].GPIOx, ports_and_pins[x].GPIO_Pin, value );

 

You might want to make a "wrapper" function which just takes the struct, breaks-out the 2 elements, and passes them to HAL_GPIO_WritePin ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Mar 25, 2024 2:19 PM UTC

Note that the GPIO_Pin parameter of HAL_GPIO_WritePin is a bitmask - not a pin number ...

 

 

/** @defgroup GPIO_pins GPIO pins
 * @{
 */
#define GPIO_PIN_0 ((uint16_t)0x0001U) /* Pin 0 selected */
#define GPIO_PIN_1 ((uint16_t)0x0002U) /* Pin 1 selected */
#define GPIO_PIN_2 ((uint16_t)0x0004U) /* Pin 2 selected */
#define GPIO_PIN_3 ((uint16_t)0x0008U) /* Pin 3 selected */
#define GPIO_PIN_4 ((uint16_t)0x0010U) /* Pin 4 selected */
#define GPIO_PIN_5 ((uint16_t)0x0020U) /* Pin 5 selected */
#define GPIO_PIN_6 ((uint16_t)0x0040U) /* Pin 6 selected */
#define GPIO_PIN_7 ((uint16_t)0x0080U) /* Pin 7 selected */
#define GPIO_PIN_8 ((uint16_t)0x0100U) /* Pin 8 selected */
#define GPIO_PIN_9 ((uint16_t)0x0200U) /* Pin 9 selected */
#define GPIO_PIN_10 ((uint16_t)0x0400U) /* Pin 10 selected */
#define GPIO_PIN_11 ((uint16_t)0x0800U) /* Pin 11 selected */
#define GPIO_PIN_12 ((uint16_t)0x1000U) /* Pin 12 selected */
#define GPIO_PIN_13 ((uint16_t)0x2000U) /* Pin 13 selected */
#define GPIO_PIN_14 ((uint16_t)0x4000U) /* Pin 14 selected */
#define GPIO_PIN_15 ((uint16_t)0x8000U) /* Pin 15 selected */
#define GPIO_PIN_All ((uint16_t)0xFFFFU) /* All pins selected */

 

 

EDIT

As @gbm suggested, calling the member of your struct something like "pinmask" would help.

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.