Skip to main content
Leonana69
Associate
Feb 27, 2024 4:53 PM UTC
Question

What's the Correct Power Supply Scheme for H725/735 VFQFPN68 Package?

Since the VFQFPN68 package doesn't provide the VDDLDO, should the chip work just with VDD/VBAT/VDDA all connected to 3v3?

Updates: during my unit test, I kept only the STM32H725 chip on the board and removed all the other components. Then I powered the chip with 3v3 to VDD/VBAT/VDDA, but the VCAP was around 100mv and I couldn't connect to the chip. However, once I supplied 1v2 to VCAP, I could connect to it. I wonder what could cause the problem, I though the chip should have an internal LDO to power the Core.

This topic has been closed for replies.

6 replies

Amel NASRI
ST Technical Moderator
Apr 1, 2024 2:38 PM UTC

Hi @Leonana69 ,

As explained in AN5419 Getting started with STM32H723/733, STM32H725/735 and STM32H730 Value
Line hardware development, "When it is not available on an external pin, VDDLDO is connected internally to VDD."

In the same document, please refer to the figure "System supply configuration" and the table "Power supply connection" to know more about required setup for VCAP.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Associate II
Sep 21, 2024 10:01 PM UTC

I don't understand why are the SMPS pins available since it can't be used to power the LDO.

Is there any way to power the MCU using the SMPS?

KDJEM.1
ST Technical Moderator
Oct 11, 2024 9:59 AM UTC

Hello @jmarino ,

 

If I have understood your comment correctly, you are asking how to connect SMPS when no available VDDLDO like as STM32H725  VFQFPN68 package.

According to AN5419 the connection for VQFPN68 package should be like shown in the figure below

KDJEM1_0-1728890606441.png

 

If I haven't understood your comment or you need further clarification please create a dedicate thread for your request.

 

Thank you.

Kaouthar  

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.