I am facing elf file not accessible error in st link utility. Using STM32L4Q5VGT6P but in IAR i am able to program and debug. But in st link this error popping up. Please suggest a solution thanks.
ST-LINK SN : B55B5A1A00000000F945F301 ST-LINK Firmware version : V2J43S7 Connected via SWD. SWD Frequency = 4000K. Target voltage = 3.3 V. Connection mode : Normal. Device ID:0x467 Device family :Unknown device
Full chip erase... Read out protection is activated
Loading file... Flash Programming: File : C:\Users\ATPL_3\Desktop\SMC_01.01.15 Firmware\SMC_01.01.15 Sample66Star.hex Address : 0x08000000 Disabling read out protection... Read out protection is activated. It will be disabled. Could not disable Read Out Protection! Memory programming... ±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±± 0% 0% The elf loader file is not accessible.