Skip to main content
JMors.1
Associate III
September 25, 2020
Solved

STM32H7B3i-DK - Inconsistency between Schematic and Users Manual for Arduino headers

  • September 25, 2020
  • 5 replies
  • 1642 views

I'm looking to use the Arduino header on the STM32H7B3i-DK, however I am finding an inconsistency between what is defined in the Schematic and what is listed in the Users Manual.

Example:

For header C10 Pins 1 and 2:

The schematic shows these mapped to MCU Pin PF10 and PI7 respectfully.

The User's Manual shows this mapped to MCU Pin PD1, PI2 respectfully

For header C11 Pin 1:

The schematic shows this mapped to PH14

The User's Manual shows this mapped to PB11

Header CN20, Pins 1, 3, and 4 do not match between the Schematic and User's Manual.

Reference:

User Manual: https://www.st.com/resource/en/user_manual/dm00610478-discovery-kit-with-stm32h7b3li-mcu-stmicroelectronics.pdf

Schematic:: https://www.st.com/resource/en/schematic_pack/mb1332-h7b3i-b02_schematic.pdf

Is there a way to verify which is the correct one?

Thanks

This topic has been closed for replies.
Best answer by JMors.1

Yeah, I had seen that, however I have a B02 version board so I was just matching the schematic to the board.

I do think the User's Manual is more likely wrong.

5 replies

TDK
September 25, 2020

> Is there a way to verify which is the correct one?

Two options:

  • Probe for continuity between the pin and the output. Easy if you have fine enough probes.
  • Set the pin as GPIO and toggle it. Measure the output with a multimeter/scope/logic analyzer.

"If you feel a post has answered your question, please click ""Accept as Solution""."
JMors.1
JMors.1Author
Associate III
September 25, 2020

I suppose I had to clarify my question.

Would it be possible that someone from ST could clarify which is correct; the User;s Manual or the Schematic, or just correct the documentation?

Andreas Bolsch
Lead III
September 25, 2020

There's already a newer schematic https://www.st.com/resource/en/schematic_pack/mb1332-h7b3i-c01_schematic.pdf

But there seems to be no difference relative to B02 regarding the Arduino connectors.

JMors.1
JMors.1AuthorBest answer
Associate III
September 25, 2020

Yeah, I had seen that, however I have a B02 version board so I was just matching the schematic to the board.

I do think the User's Manual is more likely wrong.

Mike_ST
ST Technical Moderator
September 29, 2020

Thank you for reporting.

The schematics (B02 or C01) are correct.

The User's Manual will be updated.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.