Skip to main content
Associate
Feb 12, 2026 2:01 AM UTC
Solved

STLink not appearing in Device Manager

I installed stsw-link009 on my pc so I could use the STLinkv3. The PC did not see the STLink-v3. I then installed STM32Cubeprogrammer thinking that would fix the stlink driver issue but when I look under devices USB in the device manager I can not see the stlinkv3 anywhere and the STM32CubeProgrammer doesn't see it either. The same stlinkv3 works on other pcs. Since I can't see it on my pc I can't right click it to uninstall the driver so I am not sure what to do next.

Imen.DBest answer
ST Technical Moderator
Feb 12, 2026 6:33 AM UTC

Hello @Kat1234 

Ensure you have the latest drivers and firmware.

I suggest that you review this FAQ: Possible communication failure between STLINK-V3 and some recent computers.

See also: How to solve connection errors when connecting and programming the STM32 target board.

Hope that help you!

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

5 replies

Imen.DBest answer
ST Technical Moderator
Feb 12, 2026 6:33 AM UTC

Hello @Kat1234 

Ensure you have the latest drivers and firmware.

I suggest that you review this FAQ: Possible communication failure between STLINK-V3 and some recent computers.

See also: How to solve connection errors when connecting and programming the STM32 target board.

Hope that help you!

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Andrew Neil
Super User
Feb 12, 2026 9:51 AM UTC

@Kat1234 wrote:

 when I look under devices USB in the device manager I can not see the stlinkv3 anywhere 


Do you even see an "unrecognised" device?

Does Device Manager do anything at all when you plug the STLink in?

 

If there isn't even an "unknown" devices, that suggests that the STLink is not electrically connecting to the PC at all. Drivers can't fix that!

See this post.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Kat1234Author
Associate
Feb 16, 2026 12:42 AM UTC

Thanks for your responses.  I got it working.  All the type A USB ports on the front of the PC did not even register the STLink but I had a docking station and one USB C port which I plugged in a USB C to A adaptor.  Both the docking station and the USB C port worked and I could connect to the STLink and saw it in Windows device drivers.

Andrew Neil
Super User
Feb 16, 2026 9:23 AM UTC

Yes, "try other USB ports" and "with/without hubs/docking station" are standard things to try.

Glad to hear it worked.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Kat1234Author
Associate
Feb 16, 2026 12:44 AM UTC

Thanks