Skip to main content
Associate
July 25, 2025
Solved

STDES-2KW5CH48V Firmware

  • July 25, 2025
  • 1 reply
  • 208 views

Hi All,

 

We are building a charger based on STDES-2KW5CH48V. On ST .hex file is available as firmware. 

Is source code also available ?

 

Thanks in advance.

 

Regards,

Vimal 

This topic has been closed for replies.
Best answer by Peter BENSCH

Welcome @vimalsingh126, to the community!

For security reasons, no source code is made available for such high-power applications. Also, only the design documentation is available from STDES, it is not offered for sale.

You are welcome to get in touch with your local distributor or sales contact who will help you realise your project if the quantity is large enough.

Hope that helps?

Regards
/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
August 7, 2025

Welcome @vimalsingh126, to the community!

For security reasons, no source code is made available for such high-power applications. Also, only the design documentation is available from STDES, it is not offered for sale.

You are welcome to get in touch with your local distributor or sales contact who will help you realise your project if the quantity is large enough.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.