Skip to main content
Associate II
June 25, 2024
Solved

ST-Link V2 won't connect after firmware update

  • June 25, 2024
  • 7 replies
  • 8609 views

After I updated ST-Link to firmware version V2J43S7 through STM32 Cube Programmer, I can't connect it to my laptop and program my STM32 F405 Feather board. I have attached the error message to this post.

This topic has been closed for replies.
Best answer by Techn

Try to connect while you press reset

 

7 replies

Tesla DeLorean
Guru
June 25, 2024

Is this an Authentic ST-LINK? or boot-leg one?

If you break the PA13/PA14 pin operation you won't be able to connect. Reset with BOOT0=HIGH to stop running broken user code.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
vs13Author
Associate II
June 25, 2024

It is an authentic ST-LINK! I've reset the board, but I still can't connect. How would I break the PA13/14 operation?

AScha.3
Super User
June 25, 2024

>How would I break the PA13/14 operation?

If you set (in CubeMx ) not SWD debug, but use the pins for anything else ; then no more debug, as soon, as your program starts.

Then only can use bootloader, or hard reset (connect under reset, hard reset ( setting)) to connect.

If you feel a post has answered your question, please click on " Best Answer ".