Question
ST-Link doesn't find Murata CMWX1ZZABZ-072 via SWD port
Hello,
I want to connect CMWX1ZZABZ-072 with ST-Link, but it doesn't works.
CMWX1ZZABZ-072 has a break out board which can program with arduino core.
But I want advanced programming.
So I want to program on Keil.
I tried to connect CMWX1ZZABZ-072 with ST-Link in following steps:
- Installed ST-Link utility( STSW-LINK004) and ST-Link driver(STSW-LINK009)
- Connected PC and ST-Link
- Checked that "STM32 STLink" is recognized as USB device in device manager.
- Open ST-Link utility, and install ST-Link Firmware update
- Set parameters as following screen shot
- Connect SWD ports and supplied power to MCU
- Set high BOOT0, and reset MCU
- Select "Connect" on ST-LINK utility
Then, ST-Link utility says likes this picture.
Please teach me how can I solve this problem?
My environments are here.
- ST Link v2
- Boards: Tlera Corp Grasshopper
- MCU: Murata CMWX1ZZABZ-072(Based STM32L082 )
- OS: Windows 10
- CPU: Intel(R) Xeon(R) CPU E3-1225 v6
Thanks,
Tetsuro