cancel
Showing results for 
Search instead for 
Did you mean: 

QSPI in stm32h747 cm4

ujwal_kumar_N_L
Associate II

Hi community ,
I'm currently working on STM32H747I DISCO0 Board .The peripheral I'm using is QSPI, I'm able to read/write and also enter Xip mode in CM7 .
Problem:

1)QSPI does not work in CM4 .Need to access QSPI in CM4 and perform same operations as read/write and Xip mode .
2)Please specify the Steps to be taken to work on CM4 for QSPI.

Details:
CubeIDE :Version: 1.12.1
CubeMX :6.10.0

Thank you and regards 
UJWAL KUMAR N L

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

When you enable the peripheral in CubeMX, assign it to a core.

TDK_0-1706104423242.png

You can assign it to both cores, but only one of them will initialize it. After initialization, both cores can access it, but ensure they don't try to do so at the same time.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
TDK
Super User

When you enable the peripheral in CubeMX, assign it to a core.

TDK_0-1706104423242.png

You can assign it to both cores, but only one of them will initialize it. After initialization, both cores can access it, but ensure they don't try to do so at the same time.

If you feel a post has answered your question, please click "Accept as Solution".