Skip to main content
samsarn
Associate
October 6, 2020
Question

Problem with ST-LINK programming - "failed to erase memory"

  • October 6, 2020
  • 4 replies
  • 1506 views

Hi,

ST-LINK/V2 Flash programming is not working. Board is based on STM32F303C6, tested with STM32CubeProgrammer API v2.3.0.

Target voltage shows up 1.56V, sometime less. Find Attached STM32CubeProgrammer log for reference.

Can you please tell me what would be the issue?

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
October 6, 2020

Specific details on the board design and connectivity might be more helpful...​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
samsarn
samsarnAuthor
Associate
October 6, 2020

STM32F303C6 board has own 3.3 volt LDO with SWD interface. With USB based SHIWAKI Metal ST-Link V2 debugger, the board connection and flash programming works fine. With ST-LINK/V2 [www.st.com/stlinkv2/] board not working now. Earlier it was working. I suspect there is some issue with debugger and not sure why the voltage reports 1.56V or less.

SWD - MCU connection are -

SWCLK - PA14

SWDIO - PA13

GND - GND

RESET - MCU RESET

Find below STCubeProgrammer log with different voltage reporting with only ST-Link V2 debugger connection to computer.

15:15:10 : ST-LINK SN : 48FF74066580515316330367 [ With SHIWAKI Metal ST-Link V2 debugger]

15:15:10 : ST-LINK FW : V2J37S7

15:15:10 : Voltage : 3.19V

15:15:10 : Error: No STM32 target found!

15:17:06 : Warning: Device changed, refreshing...

15:17:06 : ST-LINK SN : 35FF72064D53373251552143 [ With [www.st.com/stlinkv2/] debugger]

15:17:06 : ST-LINK FW : V2J37S7

15:17:06 : Voltage : 1.53V

15:17:06 : Error: No STM32 target found!

Uwe Bonnes
Chief
October 6, 2020

You need Stlink with level translators to talk to a device with 1.53 Volt IO voltage. But 1.53 Volt is outside the voltage specs for s F3.

samsarn
samsarnAuthor
Associate
October 6, 2020

STM32F303C6 has 3.3 volt supply. what I observe is stlink2 debugger ( [www.st.com/stlinkv2/] debugger) report voltage as 1.53.

With  USB based SHIWAKI Metal ST-Link V2 debugger - connection and flash programming works

With [www.st.com/stlinkv2/] debugger] - connection, flash read works. But Flash erase fails with "failed to erase memory" error