cancel
Showing results for 
Search instead for 
Did you mean: 

Power ON/OFF sequence OF STLINK v2 and the target device

Techn
Senior II

Hello,

Target is power from another source. STlink from USB of laptop

I was wondering if the power ON/OFF of STLINK and the target sequencing will damage either the devices? I had one STLINK v2 seems to be damaged while debugging and later it is not able to detect the target, but programmer detects the stlink serial number .. With another STlink I am able to detect the target.

0 REPLIES 0