Skip to main content
Associate II
December 2, 2024
Solved

NUCLEO-H753ZI voltage output

  • December 2, 2024
  • 1 reply
  • 975 views

Hello,

 

Can I output an adjustable voltage ranging from -10V to 10V using the h753zi development board?

 

I found something like a "PWM to 0-5V/10V DAC Module."

Would I need to use such an external module or build an additional circuit externally to achieve this?

 

I would appreciate your advice and look forward to your response.

 

Thank you!

This topic has been closed for replies.
Best answer by Peter BENSCH

As the entire NUCLEO board operates with a positive voltage, a negative output voltage can only be achieved with external circuitry, which in turn also requires a negative supply voltage.

So yes, for ±10V you would have to connect a level shifter, e.g. using opamps.

Hope that helps?

Regards
/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
December 2, 2024

As the entire NUCLEO board operates with a positive voltage, a negative output voltage can only be achieved with external circuitry, which in turn also requires a negative supply voltage.

So yes, for ±10V you would have to connect a level shifter, e.g. using opamps.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.