Skip to main content
flyer31
Senior
April 23, 2019
Question

NRST / Reset Pin in STM32H7 more ESD sensitive than in STM32F4?

  • April 23, 2019
  • 2 replies
  • 2052 views

Hi,

I have a new PCB here which somehow has latch up problems on the NRST pin quite recently. Usually then the NRST pin would just have zero DC resistance (or typically 1 Ohm) to GND. And then of course also the oscillator (8MHz XTAL) will not start working and chip keeps in reset (this is then also the error message of ST-LINK).

I use an external 10kOhm resistor against 3V3 (VCC) and then I have an about 5cm long PCB trace to the 4pin ST-LINK Debug connector... .

In the last 3 weeks I had about 5 times such a latch up problem with this PCB (STM32H750 processor, 100pin LQFP, "Y" version - this is still the startup version I think according to errata sheet...).

Now I added a 100nF capacitor to the reset line against GND. Hoping that it will be fixed now (Nucleo H743 also has such a cap, and in the datasheet they recommed it if a reset button is installed ... I do NOT have a reset button in my PCB, but maybe this cap anyhow somehow much better ... just I never had to do this with STM32F4 PCBs ... and also I never had any STM32 latchup problems before ... this is my first STM32H7 PCB...).

This topic has been closed for replies.

2 replies

Uwe Bonnes
Chief
April 24, 2019

NRST is designed to work with the chip internal pullup and an external 100 nF capacitor. With your setup with no capacitor and the external 10 k pullup, reset timing is screwed. However this should not cause breakage. Are you sure there were to ESD discharges or external voltages above 4 Volt involved?

flyer31
flyer31Author
Senior
April 24, 2019

This new PCB also has a 230V rms test circuit on board ... this is new to me ... but it is all isolated nicely with isolated supply for the 230V part (>2kV isolation voltage, 8mm creepage paths...), and I am not doing nasty things on the 230V side ... . And both circuits have no connection to PE (just standard Y decoupling capacitors...).

So due to this I cannot answer this for sure for now. Now I anyway added the 100nF capacitor ... the next PCB will be much more standard, without 230V ... when I do this (and if I have the courage to again try without 100nF cap), I can tell you more... . (but possibly I will better use the 100nF cap now always, to avoid this problem..).

PS: Meanwhile I added a 300uH - 500mA 12x12mm SMD choke in the 24V supply line for the CPU voltage supply, and now the problems seem to be fixed. This PCB is a 10A 24V DC PWM supply for a lamp ... I have no real experience such high current PWM so far ... the latch-up always happened, when my 24V supply was without current control (current control set to max limit of 11A - somehow then the 24V supply on switching on made crazy things). ... After I recognized this, I inserted the choke, and now fine (but I also added the 0.1uF in the reset line))... . I think this probably was due to this missing choke ... in "usualy PCBs" I always would use a current controlled choke for the complete PCB ... but current controlled choke for 10A would have been a bit large of course :).