Skip to main content
Associate
June 18, 2024
Question

Microcontroller dead

  • June 18, 2024
  • 2 replies
  • 1850 views

Morning everybody

The microcontroller on my nucleo board NUCLEO-H755ZI-Q is dead after i have used 5V external power to supply it. I don't understand why

2 replies

Uwe Bonnes
Chief
June 19, 2024

Read the data sheet and understand "Maximum ratings" Applying 5 Volt to an FT pin when the chip is unpowered will kill the chip as applying 5 Volt to a TT pin when powered.

FistelAuthor
Associate
June 19, 2024

Thanks

 

Please, what mean "FT pin" and  "TT pin" ?

Uwe Bonnes
Chief
June 19, 2024

Have a look at the datasheet table "Legend/abbreviations used in the pinout table"

Senior III
June 20, 2024

On which pin or connector did you apply 5v? Try to connect to usb, and see if its getting detected by cube programmer. 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Uwe Bonnes
Chief
June 20, 2024

If the MCU heats up fast, it is broken. Been there, done that 8-)

FistelAuthor
Associate
June 21, 2024

The MCU doesn't heat