2023-01-26 7:15 AM
Hello everyone,
i am planing to use an STM32 microcontroller in a project and would like to have a debugger on the same board. I then have to use another microcontroller ie. STM32F103CBT6 the same as used on STLINK-V2-1 on Nucleo boards, which will act as the debugger for the actual microcontroller. But this need to be flashed with the right firmaware to do its job.
I have searched everywere for an original firmware of STLINK-V2-1 but did not find any. How can i find an official and original Firmware for STLIN-V2-1 debugger?
Thanks alot!
Solved! Go to Solution.
2023-01-26 7:26 AM
Welcome, @MDowa.1, to the community!
The firmware for the ST-LINK is not available for self-building of the ST-LINK and is legally programmed exclusively on original ST-LINKs.
However, you can solder in the STLINK-V3MODS, which were developed directly for this purpose.
Does it answer your question?
Regards
/Peter
2023-01-26 7:26 AM
Welcome, @MDowa.1, to the community!
The firmware for the ST-LINK is not available for self-building of the ST-LINK and is legally programmed exclusively on original ST-LINKs.
However, you can solder in the STLINK-V3MODS, which were developed directly for this purpose.
Does it answer your question?
Regards
/Peter
2023-01-26 7:33 AM
Hi Peter,
thanks for fast answering.
Ok i see. Using the STLINK-V3MODS is then the best idea.
Again thank your very much! :)
2023-01-26 7:34 AM
You're welcome.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
2023-02-06 6:52 AM
<<Ignore this, appears to actually be PC side code, not STLink Firmware :(
Is this "Open Source STLINK" on Github OK to use?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.