Skip to main content
VKoga.1
Associate II
September 10, 2021
Solved

How to connect VREF+ pin on stm32F722RET6?

  • September 10, 2021
  • 2 replies
  • 1146 views

I am designing a custom PCB using STM32F722RET6. How to connect the VREF+ pin(13) on the SMT32F722RET6?.

As per the hardware development manual, it says

"The VREF+ pin can be connected to the VDDA external power supply"

and then, "VDDA=VDD and VSSA=VSS."

can I connect it to 3.3V external supply?

This topic has been closed for replies.
Best answer by Peter BENSCH

Welcome, @VKoga.1​, to the community!

yes, you can connect it to VDD. Please also read the General PCB Design Guidelines with figure 51 in the datasheet.

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

Good luck!

/Peter

2 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
September 10, 2021

Welcome, @VKoga.1​, to the community!

yes, you can connect it to VDD. Please also read the General PCB Design Guidelines with figure 51 in the datasheet.

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
VKoga.1
VKoga.1Author
Associate II
September 11, 2021

Thank you so much, like always never been let down by ST.