Skip to main content
Associate III
May 14, 2025
Question

NetXDuo Ethernet on nucleo-h753zi only works with delay

I managed to create a working example ethernet NetXDuo project for the nucleo-h753zi board based of this guide:

https://community.st.com/t5/stm32-mcus/creating-a-dual-ipv6-amp-ipv4-netxduo-udp-application-for/ta-p/570521

See my repository here:

https://github.com/mo-krauti/nucleo-h753zi-ethernet-netxduo

This only works by adding a delay before starting NetXDuo. Why could that be? I also could not find any link mentioning this online? Generally I think setting up the Ethernet Controller on H7 is quite hard compared to the F7 series.

This topic has been closed for replies.

4 replies

Andrew Neil
Super User
May 14, 2025
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
May 15, 2025

Specifically, take a look at the two posts by @Guillaume K in this thread:

https://community.st.com/t5/stm32-mcus-embedded-software/stm32f767-lwip-tcp-client/m-p/778561

@mo_krauti - do they address your issue?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mo_krautiAuthor
Associate III
May 20, 2025

I mean it works now, but this does not explain why the delay is needed and is not documented anywhere.

Andrew Neil
Super User
May 20, 2025

@mo_krauti wrote:

but this does not explain why the delay is needed 


The posts I mentioned suggest some possible reasons - so worth checking out ...

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.