Skip to main content
maciekgt
Visitor II
November 18, 2010
Question

Debugging STM32Discovery with OpenOCD

  • November 18, 2010
  • 7 replies
  • 2339 views
Posted on November 18, 2010 at 21:40

Hello

I've sadly got to know that native ST-Link built in my STM32Discovery won't work with OpenOCD. So my question is: what hardware would you suggest to connect Discovery with to use OpenOCD? Some Jtag? First question should be: is it possible to do so?

TIA

Best Regards

Maciej

#openocd-stlink #openocd #stlink #swd
This topic has been closed for replies.

7 replies

stm2399
Visitor II
January 2, 2010
Posted on January 02, 2011 at 22:03

Yes it's possible

See here

[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/ST-Link Linux Driver&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000491D59B8574F8049B5DFA3E8B21CBA51]Flat.aspx

And here

http://www.versaloon.com/bbs/viewtopic.php?f=2&t=17&start=0

/Bingo

Tesla DeLorean
Guru
November 18, 2010
Posted on November 18, 2010 at 22:50

Seems to defeat the point of having the debug hardware on the board.

You can always disconnect the SWD (CN3 jumpers, separate ST-LINK from STM32), and then wire up either your own SWD or JTAG connection to the STM32.

The schematic is here

http://www.st.com/stonline/products/literature/um/17217.pdf

Documents the connectors, and solder bridges, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
vender007
Associate
January 19, 2011
Posted on January 19, 2011 at 10:44

search for versaloon and here is a nice tutorial to use it:

https://sites.google.com/a/stf12.net/developer-sw-fw/eclipse-demo

leha2000
Visitor II
April 23, 2011
Posted on April 23, 2011 at 14:35

OpenOCD not working with STM32Discovery, but exists stlink project, which fine working with STM32Discover.

https://github.com/texane/stlink

The newest version doesn't work for me though, try this one:

https://github.com/whitequark/stlink/commit/d1c3176f3a7cdbd7a0c4df832c627bc508a75296

It works:

For compile cut -Werror in build/Makefile,

add to gcc options

-Wl,--section-start=.text=0x8000000 \ #for load to flash

or

-Wl,--section-start=.text=0x20000000 \ #for load to SRAM

or change you ldscript

and read README.

 

sjo2
Visitor II
May 8, 2012
Posted on May 08, 2012 at 21:05

This an old thread but still quite relevant.

OpenOCD does now support the stlink, both stlink/v1 and stlink/v2.

Board config's exist for all current discovery boards and standalone dongles.:

stm32f0discovery, stm32f4discovery, stm32ldiscovery, stm32vldiscovery.

Cheers

Spen

frankmeyer9
Associate III
May 9, 2012
Posted on May 09, 2012 at 10:53

OpenOCD does not support SWD at all, at least up to now. So are at least my latest information.

Or am I wrong here ?

sjo2
Visitor II
July 4, 2012
Posted on July 04, 2012 at 10:32

SWD is only supported in OpenOCD when using the stlink adapter.

Spen