Skip to main content
Associate III
October 15, 2024
Question

Couldn't write and read EEPROM on STM32L0538-Discovery

Hello,

I  tried to EEPROM write/read test but it seems to not have written into EEPROM normally.

My defined functions corresponding to EEPROM are like following.

#define FLASH_USER_START_ADDR ((uint32_t)0x8008000)
#define FLASH_USER_END_ADDR ((uint32_t)0x800A000)

void eeprom_write_Word(uint32_t address, uint32_t value)
{
if(!IS_FLASH_DATA_ADDRESS(address))
{
return;
}
HAL_FLASHEx_DATAEEPROM_Unlock();
HAL_FLASHEx_DATAEEPROM_Program(FLASH_TYPEPROGRAMDATA_WORD, address, value);
HAL_FLASHEx_DATAEEPROM_Lock();
}

void eeprom_read_Word(uint32_t address, uint32_t* value)
{
if(!IS_FLASH_DATA_ADDRESS(address))
{
return;
}
*value = *(__I uint32_t*)address;
}

And write/read lines in main are

eeprom_write_Word(FLASH_USER_START_ADDR, 1);
HAL_Delay(100);
eeprom_read_Word(FLASH_USER_START_ADDR, eeprom_buf);

As result buffer was empty.

How could I write and read normally?

Thanks

    This topic has been closed for replies.

    9 replies

    Andrew Neil
    Super User
    October 15, 2024
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Peter BENSCH
    ST Technical Moderator
    October 15, 2024

    +1 for the hint of @Andrew Neil 

    @curiae Did you try the suggestion of @dmeehan in this thread?

    Regards
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    curiaeAuthor
    Associate III
    October 15, 2024

    Hello,

    I think you mean about Edit/code so I'll ask again.

    I tried to EEPROM write/read test but it seemed to not have written into EEPROM normally.

    My test code  are like following.

    As result buffer was empty.

    How could I write and read normally?

    Thanks

    #define FLASH_USER_START_ADDR ((uint32_t)0x8008000)
    #define FLASH_USER_END_ADDR ((uint32_t)0x800A000)
    
    void eeprom_write_Word(uint32_t address, uint32_t value)
    {
     if(!IS_FLASH_DATA_ADDRESS(address))
     {
     return;
     }
     HAL_FLASHEx_DATAEEPROM_Unlock();
     HAL_FLASHEx_DATAEEPROM_Program(FLASH_TYPEPROGRAMDATA_WORD, address, value);
     HAL_FLASHEx_DATAEEPROM_Lock();
    }
    
    void eeprom_read_Word(uint32_t address, uint32_t* value)
    {
     if(!IS_FLASH_DATA_ADDRESS(address))
     {
     return;
     }
     *value = *(__I uint32_t*)address;
    }
    
    int main(void)
    {
     HAL_Init();
     SystemClock_Config();
     MX_GPIO_Init();
     MX_RTC_Init();
     eeprom_write_Word(FLASH_USER_START_ADDR, 1);
     HAL_Delay(100);
     eeprom_read_Word(FLASH_USER_START_ADDR, (uint32_t*)test_buf);
     uint32_t test_dat = test_buf[0];
     while(1)
     {}
    }

     

     

    Andrew Neil
    Super User
    October 15, 2024

    You are not checking any of the return codes from any of the HAL functions - that would be the first thing to do.

    Also, your code can return silently and do nothing:

    void eeprom_read_Word(uint32_t address, uint32_t* value)
    {
     if(!IS_FLASH_DATA_ADDRESS(address))
     {
     return;
     }
     *value = *(__I uint32_t*)address;
    }

    So if the IS_FLASH_DATA_ADDRESS test fails, that function gives you no indication at all of the error!

     

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Sco
    ST Employee
    October 16, 2024
    curiaeAuthor
    Associate III
    October 16, 2024

    Hello,

    I think it's a general explanation document about EEPROM.

    Could you show me some sample sources for EEPROM read/write?

    Thanks

     

    Shirley.Ye
    ST Employee
    November 1, 2024

    Hello,

     

    you need to check if the function HAL_FLASHEx_DATAEEPROM_Program executed successfully.

     

    for example,

     

    // Unlock the EEPROM memory for writing

    HAL_FLASHEx_DATAEEPROM_Unlock(); // Write data to EEPROM

    if (HAL_FLASHEx_DATAEEPROM_Program(FLASH_TYPEPROGRAMDATA_WORD, address, writeData) == HAL_OK)

    {

    // Read data from EEPROM
    readData = *(__IO uint32_t*)address;

    // Check if the read data matches the written data

    if (readData == writeData)

    {

    // Data matches

    } else {

    // Data does not match
    }

    }

    // Lock the EEPROM memory to prevent further writing

    HAL_FLASHEx_DATAEEPROM_Lock();