cancel
Showing results for 
Search instead for 
Did you mean: 

Control GPIO of STLINK-V3SET?

Simon Nilsson
Associate

The product page for  STLINK-V3SET lists the following:

Multi-path bridge USB to SPI/UART/I2C/CAN/GPIOs

I can see in the STM32CubeProgrammer CLI that use can use the SPI/I2C/CAN/UART functions. But can you control the state of the GPIO 0-3 pins in some way?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
LSimc.1
Associate

It would be greatly appreciated if someone could assist with the following matter: I have also been unable to find any references or guides describing the process for controlling the GPIOs of the ST-link V3 using the CLI interface.

Is it even possible?

Thanks