Skip to main content
August 10, 2020
Question

[BUG] St-Link is not detected after installing STM32CubeIDE V 1.4.0.

  • August 10, 2020
  • 16 replies
  • 7401 views

I was normally using STM32CubeIDE V 1.3.0 and St-Link was working.

The St-Link firmware is updated.

The St-Link Utility (V 4.4.0.0 and V 4.5.0.0) finds and connects to the St-Link correctly.

Whenever a new IDE version becomes available, will the user have to ask for help to make St-Link work? :|

Can the IDE itself update St-Link? (Or at least report the problem correctly?)

This topic has been closed for replies.

16 replies

Cartu38 OpenDev
Graduate II
August 11, 2020

Help > Check for Updates ... STM32CubeIDE 1.4.1 is solving trouble.​

August 12, 2020

Thanks, this update I did right after installation. Still not working.

HPham.1590
Associate III
August 12, 2020

Hi,

As my experience, I got the same issue when update from 1.3 to 1.4 version.

In CubeIDE 1.4, we need to install STM32Cube Programmer, I'm not sure but I think CubeIDE1.4 use Cube Programmer as default software to run task.

You can download this software here https://www.st.com/en/development-tools/stm32cubeprog.html

Hieu

August 12, 2020

Thank you, I saw your answer just now. I had already downloaded CubeMX and Prog, it really worked. What a pity, too bad, making an IDE of this size but depends on other software.

HPham.1590
Associate III
August 12, 2020

Cube is an ST's Ecosystem, it includes CubeIDE, CubeMX and CubeProgrammer, so I think that's business strategy =)))

Hieu

August 12, 2020

I did some tests (following the order quoted, in sequence):

  • After installing STM32CubeIDE 1.4, ST-Link V2 did not work (as mentioned above).
  • After installing STM32CubeMX 6.0, STM32CubeIDE 1.4 worked with ST-Link V2 (as already mentioned above).
  • After uninstalling STM32CubeMX 6.0, STM32CubeIDE 1.4 continued to work with ST-Link V2.
  • After uninstalling STM32CubeIDE 1.4 and installing STM32CubeIDE 1.4 again, ST-Link V2 stopped working.
  • After installing STM32CubeMX 6.0, STM32CubeIDE 1.4 still did not work with ST-Link V2.
  • After installing STM32CubeProgrammer 2.5, STM32CubeIDE 1.4 still did not work with ST-Link V2.

So it's not just that yet. I did something else.

August 12, 2020

And it still doesn't work.

I found another post with several users with the same problem:

Some say it is a matter of using HUB, but it has nothing to do with it, since version 1.3 works without problems.

https://community.st.com/s/question/0D53W00000Di9H7SAJ/stlink-not-found-when-debugging-with-stm32cubeide-140

August 12, 2020

I found another post, citing OpenOCD.

https://community.st.com/s/question/0D50X0000BVnlm0/debugger-not-working-after-upgrade-to-stm32cubeide-110

I tried and worked the ST-Link with OpenOCD.

It seems to be a problem with GDB Server, it seems that IDE 1.4 does not work properly with GDB Server.

Download pre-built OpenOCD for Windows:

https://gnutoolchains.com/arm-eabi/openocd/

Hchao.1
Visitor II
August 19, 2020

C:\ST\STM32CubeIDE_1.3.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_1.3.0.202002181050\tools\bin>ST-LINK_gdbserver.exe -d -v -e -cp "C:\ST\STM32CubeIDE_1.3.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_1.3.0.202002181050\tools\bin"

use this command ,it works fine.just run the bat file,and then can debug as normal.

Hchao.1
Visitor II
August 19, 2020

0693W000003PhrAQAS.png0693W000003Phr5QAC.png0693W000003Phr0QAC.png0693W000003PhqvQAC.png

August 19, 2020

I think version 1.4 is different, it doesn't have all these files.

Hchao.1
Visitor II
August 19, 2020

you can install v1.3.0, then update to 1.4.2